MusicTech
  • Challenges & Projects
  • Design Challenges
  • MusicTech
  • More
  • Cancel
MusicTech
Forum Percussion
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 6 subscribers
  • Views 2882 views
  • Users 0 members are here
Related

Percussion

Workshopshed
Workshopshed over 11 years ago

If someone is looking for a good way to do a drum type input to their project I can also recommend this circuit I found earlier in the year. It works nicely with some LM393 comparators.

 

image

 

Enchanted Objects Design Challenge - Knock Knock

http://www.scienceprog.com/thoughts-on-interfacing-piezo-vibration-sensor/

  • Sign in to reply
  • Cancel

Top Replies

  • DAB
    DAB over 11 years ago +1
    Interesting. I happen to have some LM393 chips. I might have to dig them out and try this circuit. Thanks DAB
Parents
  • D_Hersey
    D_Hersey over 10 years ago

    Sorry, I am not sure what the Zeners are for.  Nor do I know Vcc.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Workshopshed
    Workshopshed over 10 years ago in reply to D_Hersey

    The zeners are there to clip the signal as it could go higher than the input range of the comparator. It's explained in some detail in the link from the original post.

     

    Vcc is the postive power rail, which was +5v in my case. The logic levels on the beaglebone are lower, at 3.3v so you would want to use a lower level supply and also 3.3v zener diodes if you were to adapt the circuit for this challenge. The LM393 would work at that lower voltage without issue.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Workshopshed
    Workshopshed over 10 years ago in reply to D_Hersey

    The zeners are there to clip the signal as it could go higher than the input range of the comparator. It's explained in some detail in the link from the original post.

     

    Vcc is the postive power rail, which was +5v in my case. The logic levels on the beaglebone are lower, at 3.3v so you would want to use a lower level supply and also 3.3v zener diodes if you were to adapt the circuit for this challenge. The LM393 would work at that lower voltage without issue.