MusicTech
  • Challenges & Projects
  • Design Challenges
  • MusicTech
  • More
  • Cancel
MusicTech
Forum Percussion
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 6 subscribers
  • Views 2882 views
  • Users 0 members are here
Related

Percussion

Workshopshed
Workshopshed over 11 years ago

If someone is looking for a good way to do a drum type input to their project I can also recommend this circuit I found earlier in the year. It works nicely with some LM393 comparators.

 

image

 

Enchanted Objects Design Challenge - Knock Knock

http://www.scienceprog.com/thoughts-on-interfacing-piezo-vibration-sensor/

  • Sign in to reply
  • Cancel

Top Replies

  • DAB
    DAB over 11 years ago +1
    Interesting. I happen to have some LM393 chips. I might have to dig them out and try this circuit. Thanks DAB
Parents
  • D_Hersey
    D_Hersey over 10 years ago

    Why not omit D1?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Workshopshed
    Workshopshed over 10 years ago in reply to D_Hersey

    Don Hersey wrote:

     

    Why not omit D1?

    That's a good question, you probably should ask the designer of the circuit, I'd guess that it's either because the behaviour of the diodes is not symmetrical or because it provides 2 paths of protection.

     

    It's definitely not the only solution, but it did work nicely in my case and it should also (with the above adjustment for 3.3v) work for this challenge.

     

    voltage clipping - How would I design a protection clipper circuit for ADC input? - Electrical Engineering Stack Exchang…

    Protecting Inputs in Digital Electronics | DigiKey

    Microcontroller Input Protection Techniques - Kevin's Projects

     

    If you have a oscilloscope you could try different options and let us know if there is a difference or not.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 10 years ago in reply to Workshopshed

    Normally schottky diodes are used in this configuration instead of zeners - they provide better clamping and it doesn't matter what the rail voltage is. As you mentioned, a zener could be used to eliminate one diode in a specific voltage scenario, if it helps with the cost.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Workshopshed
    Workshopshed over 10 years ago in reply to dougw

    I read that schottky diodes are used because they have a lower threshold voltage of 0.2v

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 10 years ago in reply to Workshopshed

    You are correct Andy - they clamp before the internal protection diodes of the chip, which would typically conduct at about 0.7 volts, so the Schottky diodes take the current instead and the chip is not stressed. If you want to rely on the internal diodes and eliminate the external diodes, check that internal diodes exist, then check their current rating, then place a resistor in series with the input to ensure the current does not exceed the rating. This is still not considered good design practice, but if you are stuck without diodes and need to get it working, it should work.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • dougw
    dougw over 10 years ago in reply to Workshopshed

    You are correct Andy - they clamp before the internal protection diodes of the chip, which would typically conduct at about 0.7 volts, so the Schottky diodes take the current instead and the chip is not stressed. If you want to rely on the internal diodes and eliminate the external diodes, check that internal diodes exist, then check their current rating, then place a resistor in series with the input to ensure the current does not exceed the rating. This is still not considered good design practice, but if you are stuck without diodes and need to get it working, it should work.