On the Line
  • Challenges & Projects
  • Design Challenges
  • On the Line
  • More
  • Cancel
On the Line
Forum Green Brain - Part I - CAN bus introduction
  • News
  • Projects
  • Forum
  • DC
  • Leaderboard
  • Files
  • Members
  • More
  • Cancel
  • New
Join On the Line to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 38 subscribers
  • Views 320 views
  • Users 0 members are here
  • design challenge
  • On the line design challenge
  • can bus
  • e14-on-the-line
  • uno q
  • arduino
Related

Green Brain - Part I - CAN bus introduction

saramic
saramic 5 months ago

My first forum post for the element14 On the line smart industry themed Design Challenge.

The Idea

Plants and kids Girl are nice addition to the homeliness of a home House with garden. Sometimes you need to take the kids on holidays Island️ and how do you keep the plants at home watered? Enter the Green Brain a smart watering system. Although my premise is to have a smart pot plant watering system for when no one is around, to keep in tune with the “industry theme” I will dive into some industry standards like CAN bus - Controller Area Network (CAN bus). Using this I hope to connect a multi-node system to an Arduino UNO Q as the central host computer. Throw in some computer vision and edge AI to help orchestrate an industrial level green house, maybe even a water cannon Gun.

Pre hardware

Although I was lucky enough to have been announced as one of 10 challengers to receive some free hardware, As I live on the other side of the world Earth asia my kit has not arrived yet, so I thought it would be timely to get started anyway.

The main elements of the On-the-line challenge seem to be:

  1. Arduino UNO Q

    Single Board Computer, Arduino UNO Q, QRB2210/STM32U585, 2GB, ARM Cortex-A53/M33F

  2. MAX33041ESHLD#

    Shield Evaluation Kit, MAX33041E, Interface, CAN Transceiver

I was intruiged by the UNO Q by a review by @skruglewicz

  • Test out Arduino’s Uno Q - The new Single-Board Computer

So I purchased one a few weeks back. The CAN Transceiver board was a bit out of my price bracket, but I worked out I can get cheap, less industrial, CAN bus modules based on MCP2515 so I got a few of those to get my head around the communications standard.

CAN bus edge nodes

Given my idea was a green house, I got some DHT11 temperature/humidity sensors, and YL-69 soil hygrometer sensors. Being a CAN “bus” I decided to start by creating some simple edge nodes powered by an Arduino Nano. The idea being that each node would take a measurement and send it across the CAN bus to the central host computer (UNO Q)

Simple CAN loopback

Using the MCP2515 Arduino library, I got the following “loopback mode” test code.

// NOTE abirdged code to only show important parts
#include <mcp2515.h>

#define MCP_CS_PIN 10
#define NODE_ID    1
#define CAN_CLOCK  MCP_8MHZ

// Setup the mcp2515 device
MCP2515 mcp2515(MCP_CS_PIN);

void setup() {
    mcp2515.reset();

    ...

    // Set the speed to 500Kbps and the clock to 8MHz as per crystal
    if (mcp2515.setBitrate(CAN_500KBPS, CAN_CLOCK) != MCP2515::ERROR_OK) {
        Serial.println(F("ERR: setBitrate failed — check SPI wiring"));
        while (true);
    }

    // set it in loopback mode for testing
    mcp2515.setLoopbackMode();
}

...

void loop() {
    delay(2000);

    ...

    can_frame tx = buildFrame(temp, hum, ok);
    // Send a message
    MCP2515::ERROR sendErr = mcp2515.sendMessage(&tx);
    if (sendErr != MCP2515::ERROR_OK) {
        // code 2=ALLTXBUSY: TX buffers all stuck — chip probably in CONFIG mode
        // code 4=FAILTX: frame sent but no ACK (expected in normal mode, no bus)
        Serial.print(F("ERR: send failed code=")); Serial.println(sendErr);
        return;
    }
    printFrame("TX ", tx);

    delay(10);
    can_frame rx;
    // Read the message, will come from loopback, so same one we sent above
    if (mcp2515.readMessage(&rx) == MCP2515::ERROR_OK) {
        printFrame("RX ", rx);
        Serial.println(F("  [loopback OK]"));
    } else {
        Serial.println(F("ERR: loopback RX failed"));
    }
}

And here I got stuck for a long time, trusting my wiring and not trusting the code. In the end I worked out I had been doing too much UART recently where you connect RX from one side to TX on the other, in this case I had misconnected by MOSI (Master Out Slave In) and MISO (Master In Slave Out) SPI (Serial Peripheral Interface), MOSI → MOSI, same same. Once the wiring got fixed, I was getting the expected loopback message repeating what I was sending.

Missing from the above sketch are some initial verification and the frames for the CAN bus communications.

CAN verification

At startup, you can also verify the setup of the MCP2515 CAN bus device

// acquires the SPI bus and configures it: 10 MHz clock, most-significant bit
// first, clock polarity/phase mode 0 (idle low, sample on rising edge). This
// matches MCP2515's requirements.
SPI.beginTransaction(SPISettings(10000000, MSBFIRST, SPI_MODE0))

// asserts chip select (pulls CS low), which tells the MCP2515 "the next
// bytes on the bus are for you." Without this, the chip ignores SPI traffic.
digitalWrite(MCP_CS_PIN, LOW)

// sends the MCP2515 READ command byte (0x03). This tells the chip: "I want
// to read a register."
SPI.transfer(0x03)

// sends the register address 0x0E, which is CANSTAT (CAN Status Register).
// The chip now knows which register to return.
SPI.transfer(0x0E)

// sends a dummy byte (0x00) to clock out the register value. SPI is
// full-duplex, so you must send something to receive something; the chip
// responds with the CANSTAT byte while you transmit the dummy.
uint8_t canstat = SPI.transfer(0x00)

// de-asserts chip select, ending the SPI transaction with this chip.
digitalWrite(MCP_CS_PIN, HIGH)

// releases the SPI bus so other devices can use it.
SPI.endTransaction()

CANSTAT tells us:

The bits [7:5] of CANSTAT encode the current operating mode:

  • 0x00 → Normal mode (actively on the CAN bus)
  • 0x40 → Loopback mode (internal loopback for testing)
  • 0x80 → Configuration mode (used during init to set baud rate, masks, etc.)

This acts as a verification block for the MCP2515 setup.

8 byte CAN frame payload

To send data on CAN bus it needs to be organised in 8 bytes of payload. This is baked into the protocol at the hardware level and the MCP2515 and every other CAN controller enforces it.

The reasons CAN was designed this way is:

  • Real-time determinism — CAN was designed for automotive/industrial control systems where latency guarantees matter more than throughput. Short fixed-size messages mean worst-case bus time is predictable.
  • Bus arbitration — multiple nodes share one wire and arbitrate per-message. Long messages hold the bus and block higher-priority nodes for longer.
  • Error detection — the built-in CRC and bit-stuffing scheme works on bounded-length frames. Longer frames would need a different (heavier) error model.

For the sake of starting, I came up with the following frame layout

Byte Field Detail
0 Node ID Which sensor node sent this (e.g. 1, 2)
1–2 Temperature Big-endian uint16, scaled ×10 (e.g. 23.4°C → 0x00EA)
3–4 Humidity Big-endian uint16, scaled ×10 (e.g. 65.1% → 0x028B)
5 Status flags bit 0 = sensor OK, bit 1 always set (protocol version marker?)
6 Sequence Rolling counter, wraps 0–255, detects missed messages
7 Checksum XOR of bytes 0–6, detects corruption

The CAN ID is 0x100 + NODE_ID, so node 1 sends on 0x101, node 2 on 0x102, etc. — letting receivers filter by ID without parsing the payload.

For the time being I was not yet using the YL-69 soil hygrometer, only the DHT11 temperature/humidity sensor. The temperature and humidity is ×10 scaled to pack a float into 2 bytes, big-endian uint16. I have an XOR checksum in the 8th byte) and everything for the time being fits into an 8-byte box. Going forward I could split readings across multiple data frames or I might be able to use CAN FD, a newer standard that allows up to 64 bytes.

The code to create the frame

can_frame buildFrame(float temp, float hum, bool sensorOk) {
    can_frame frame;
    frame.can_id  = 0x100 + NODE_ID;
    frame.can_dlc = 8;

    uint16_t tempRaw = sensorOk ? (uint16_t)(temp * 10) : 0;
    uint16_t humRaw  = sensorOk ? (uint16_t)(hum  * 10) : 0;

    frame.data[0] = NODE_ID;
    frame.data[1] = (tempRaw >> 8) & 0xFF;
    frame.data[2] =  tempRaw       & 0xFF;
    frame.data[3] = (humRaw  >> 8) & 0xFF;
    frame.data[4] =  humRaw        & 0xFF;
    frame.data[5] = (sensorOk ? 0x01 : 0x00) | 0x02;
    frame.data[6] = sequence++;

    uint8_t chk = 0;
    for (int i = 0; i < 7; i++) chk ^= frame.data[i];
    frame.data[7] = chk;

    return frame;
}

and to print an incoming frame

void printFrame(const char* prefix, const can_frame& f) {
    Serial.print(prefix);
    Serial.print(F("ID:0x")); Serial.print(f.can_id, HEX);
    Serial.print(F(" node:")); Serial.print(f.data[0]);
    float t = ((uint16_t)(f.data[1] << 8) | f.data[2]) / 10.0;
    float h = ((uint16_t)(f.data[3] << 8) | f.data[4]) / 10.0;
    Serial.print(F(" T:")); Serial.print(t, 1); Serial.print(F("C"));
    Serial.print(F(" H:")); Serial.print(h, 1); Serial.print(F("%"));
    Serial.print(F(" seq:")); Serial.print(f.data[6]);
    Serial.print(F(" chk:0x")); Serial.println(f.data[7], HEX);
}

Success

I had 2 Arduinos connected by 2 wire CAN bus with a 120Ω terminator resistor (to prevent signal reflection) sending temperature and humidity readings and via a serial monitor on one of them I could see the TX, transmitted values and RX, received values from the other edge node.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

The video above has NODE 2 on the left and NODE 3 on the right.

  1. As I bring the soldering iron next to NODE 3 DHT11, the temperature starts to climb to over 30°C.
  2. Unpligging the DHT11 on NODE 2, results in 0°C being sent.
  3. Unplugging the DHT11 on NODE 3, which is the one connected to the serial monitor, results in an error connecting to the device, maybe that should also be sent across the CAN bus for when a node is not behaving.

Next

My gear is on it’s way so there will no doubt be an unboxing. But I also need to hook up my UNO Q to the above CAN bus. I did some investigation and it seems the MCP2515 devices I got are 5V whilst the UNO Q is 3V3, so I have some logic shifters coming as well as some some 3V3 logic CAN transceivers based around SN65HVD230.

I was hoping to just connect the UNO Q MPU (Microprocessor Unit, the Linux box) straight through to the CAN transceiver, but it seems that the MPU has no GPIO connections.

# wishful thinking - WILL NOT WORK

# Install can-utils if not present
sudo apt-get install -y can-utils

# Load CAN kernel modules
sudo modprobe can
sudo modprobe can_raw
sudo modprobe can_dev
sudo modprobe mcp251x

export CAN_BITRATE=500000       # must match firmware (CAN_500KBPS)
export MCP_OSCILLATOR=8000000   # 8 MHz crystal on the MCP2515 module

# NOTE: this is what presumably CANNOT be done on an UNO Q as the MPU has no
#       access to GPIO pins
export MCP_INT_GPIO=25          # GPIO pin wired to MCP2515 INT

# check for available SPI devices
ls /dev/spi*

# add a device tree overaly
#   If dtoverlay is not available, create a .dtbo manually.
#   See: https://docs.kernel.org/devicetree/overlay-notes.html
sudo dtoverlay mcp2515-can0 \
  oscillator=${MCP_OSCILLATOR} \
  interrupt=${MCP_INT_GPIO}

# check device is present
ip link show can0 &>/dev/null

# Bring up the CAN interface
sudo ip link set can0 down 2>/dev/null || true
sudo ip link set can0 up type can bitrate ${CAN_BITRATE}

echo "can0 up at ${CAN_BITRATE} bps"

# Quick sanity check, listening for 5 seconds
timeout 5 candump can0 || true

echo ""
echo "=== Setup complete ==="
echo "Run the bridge:  cd bridge && npm start"

As presumably the above will not work as there are no GPIO pins to wire the MCP2515 to have access to the Linux MPU, this means I will need the MCU (Microcontroller Unit, STM32U585) to connect to the CAN transceiver via JDIGITAL pins and then have the MPU talk to the MCU via /dev/spidev0.0 - I hope Fingers crossed.

At some point I hope to get into some computer vision and plant detection using a model like YOLOv8 or similar running no the UNO Q.

Source

https://github.com/saramic/green-brain

  • Sign in to reply
  • Cancel
Parents
  • DAB
    DAB 5 months ago

    Nice test.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • DAB
    DAB 5 months ago

    Nice test.