On the Line
  • Challenges & Projects
  • Design Challenges
  • On the Line
  • More
  • Cancel
On the Line
Forum Smart Ventilation Motor Monitoring System #2 Industrial Sensor- Omega HX94C sensor for On-the-line
  • News
  • Projects
  • Forum
  • DC
  • Leaderboard
  • Files
  • Members
  • More
  • Cancel
  • New
Join On the Line to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 38 subscribers
  • Views 225 views
  • Users 0 members are here
  • On the line design challenge
Related

Smart Ventilation Motor Monitoring System #2 Industrial Sensor- Omega HX94C sensor for On-the-line

fyaocn
fyaocn 3 months ago

image

1 Product Overview

The HX94 Series​ is a line of duct-mount RH/temperature transmitters designed for reliable, low-cost environmental monitoring in HVAC and industrial applications. It features a robust stainless steel housing, solid-state sensors for fast response, and versatile output options for easy integration. There have many types of sensors, this Omega HX94 is top niche especially for industrial. Go deep for what it is
image
With key features
Feature
Description
Benefit
Dual Sensing​
Combines Thin-Film Polymer Capacitor​ (RH) and 100Ω Platinum RTD​ (Temp) in one unit.
Simplifies installation, reduces cost versus separate sensors.
Stainless Steel NEMA 4 Enclosure​
IP66 equivalent, corrosion-resistant housing.
Suitable for harsh environments, ducts, and wet conditions. But not for dip into water, 
unboxing pic shows why.
Removable & Adjustable​
Includes removable sensor filter for cleaning and a variable-depth (1-9") duct flange.
Easy maintenance and adaptability to different duct wall thicknesses.
Linearized Outputs​
Available in 4-20 mA​ (HX94C) or 0-1 Vdc​ (HX94V).
Direct compatibility with most PLCs, DDCs, and control systems without complex scaling.
Fast Response​
RH time constant <20-30 seconds in moving air.
Quickly reflects changes in environmental conditions.

The type HX94C is for current signal and HX94V is for voltage signal. the tye in hand is HX94C.

Refer to Omega HX94C. Datasheet.pdf

2 What inside ?

Remove the cap
image
Get closer,
image
take the whole sensor out from rear end
image
magnified with PCB 
imageimageimageimage
Nice and neate
image

3 Esay to install

Gasket flange is provide for easy install
image
there is tip, one rubber ring in the middle can expand under pressure to clamp the metal enclosure, clever design.
image
water tight connectors
image

4 Technical Specifications Analysis

The data is more persuasive as such,

Relative Humidity Sensing

  • Sensor Type:​ Thin-Film Polymer Capacitor.
  • Range:​ 3% to 95% RH.
  • Accuracy:​ ±2% RH​ (Excellent for its class).
  • Repeatability:​ ±1% RH.
  • Compensation:​ -20°C to 85°C (Wide temperature compensation range ensures accuracy across operating conditions).
  • Output:​ 4-20 mA or 0-1 Vdc, linearly proportional to 0-100% RH.

Temperature Sensing

  • Sensor Type:​ 100Ω Platinum RTD (DIN 43760 standard).
  • Range:​ 0°C to 100°C (32°F to 212°F).
  • Accuracy:​ ±0.6°C (±1°F)​ (Good for HVAC applications).
  • Repeatability:​ ±0.3°C.
  • Output:​ 4-20 mA or 0-1 Vdc for the temperature channel (HX94C/V models).

Electrical & Mechanical

  • Power Supply:​ 6 to 30 Vdc (Polarity Protected). Flexible for use with 12V or 24V systems.
  • Connection Types:​ Multiple options (4-pin connector, lead wires, or 1/2" NPT with cable) provide mounting versatility.
  • Time Constant (Temp):​ 60% response time is specified, indicating a slightly slower thermal response compared to the RH sensor.

5 Apply the power source

Apply 12VDC to pin 1 and GND to Pin 2
image

the reading is 12.17V DC

image

while the current get is jus 0.01mA to pin 3

image

and 0.01-0.02mA in pin 4.

image

Here is how to connect it.

image

Ehn, this is still can not solved yet. But, this sensor is not used in the plan.Jus share it.

  • Sign in to reply
  • Cancel

Top Replies

  • saramic
    saramic 3 months ago +1
    Fantastic post and great to see the tear down - although not integral to my project will likely use it and good to know it is not to hard to get going - thank you and good luck
Parents
  • saramic
    saramic 3 months ago

    Fantastic post and great to see the tear down - although not integral to my project will likely use it and good to know it is not to hard to get going - thank you and good luck Four leaf clover 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • saramic
    saramic 3 months ago

    Fantastic post and great to see the tear down - although not integral to my project will likely use it and good to know it is not to hard to get going - thank you and good luck Four leaf clover