Path II Programmable
  • Challenges & Projects
  • Design Challenges
  • Path II Programmable
  • More
  • Cancel
Path II Programmable
Blog apt/apt-get commands not working
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
  • Author Author: buffteethr
  • Date Created: 9 Dec 2019 1:18 AM Date Created
  • Views 3487 views
  • Likes 1 like
  • Comments 6 comments
Related
Recommended

apt/apt-get commands not working

buffteethr
buffteethr
9 Dec 2019

I am on the final stages of the PetaLinux labs and about to start my project. Unfortunately, the apt and apt-get commands are not working and I cannot find away to install the commands. Any help would be appreciate. I need these commands for my project because I have to install opencv and other packages.

  • Sign in to reply
Parents
  • buffteethr
    buffteethr over 6 years ago

    Experiment 2: Secure Remote Login and File Transfer of Connect with Ultra96 Using Wi-Fi – Lab 3 recommends Filezilla. It is not present in the petalinux build so in the lab it instructs us to install Filezilla using the command: $ sudo apt install filezilla

     

    I get a command not found error.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ralphjy
    ralphjy over 6 years ago in reply to buffteethr

    FileZilla is installed on Ubuntu in the VM, not on the Ultra96. apt should work in Ubuntu.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • buffteethr
    buffteethr over 6 years ago in reply to ralphjy

    Awwww. Thanks...I have done builds on the hardware itself. I assumed that was being done here. Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • buffteethr
    buffteethr over 6 years ago in reply to ralphjy

    Awwww. Thanks...I have done builds on the hardware itself. I assumed that was being done here. Thanks.