Path II Programmable
  • Challenges & Projects
  • Design Challenges
  • Path II Programmable
  • More
  • Cancel
Path II Programmable
Blog Growing Old waiting on SDK to start
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
  • Author Author: dcsoutherner
  • Date Created: 22 Oct 2019 8:56 PM Date Created
  • Views 1007 views
  • Likes 4 likes
  • Comments 5 comments
Related
Recommended

Growing Old waiting on SDK to start

dcsoutherner
dcsoutherner
22 Oct 2019

It's been a little over 10 minutes (according to my cellphone's clock) since I clicked "Launch SDK"  from Vivado and the progress bar is almost halfway filled.

I'm following the tutorials in the "MPSoC_HW_2018_3_student_complete" zip file, the "Lab_instructions" directory.  This is lab 2, page 24.

This is on a machine with and Intel Core I7-3770 rated at 3.4 Ghx, 16 GB of memory running Ubuntu 18.04.3 LTS 64-bit.

Seriously?????

I'm supposed to create software with tools that have greater than 10 minute load times?

This is demotivating and annoying.

  • Sign in to reply
Parents
  • cmelement14
    cmelement14 over 6 years ago

    It didn't take that much time even on my VM, but I am using Ubuntu 16.04 not 18.04. It seems something not quite right to me.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • cmelement14
    cmelement14 over 6 years ago in reply to cmelement14

    Update: The same thing occurred on my VM today. I didn't wait for 10 minutes (probably 2 to 3 minutes before I shutdown the VM). After rebooting the VM and re-start the SDK, everything works again. I think the SDK may have a bug (or may be inherited from Eclipse).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • cmelement14
    cmelement14 over 6 years ago in reply to cmelement14

    Update: The same thing occurred on my VM today. I didn't wait for 10 minutes (probably 2 to 3 minutes before I shutdown the VM). After rebooting the VM and re-start the SDK, everything works again. I think the SDK may have a bug (or may be inherited from Eclipse).