Path II Programmable
  • Challenges & Projects
  • Design Challenges
  • Path II Programmable
  • More
  • Cancel
Path II Programmable
Blog Install an Ubuntu Virtual Machine
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
  • Author Author: buffteethr
  • Date Created: 13 Oct 2019 7:54 PM Date Created
  • Views 1615 views
  • Likes 3 likes
  • Comments 8 comments
Related
Recommended

Install an Ubuntu Virtual Machine

buffteethr
buffteethr
13 Oct 2019

I installed the Vivado tools in Windows when I went through other tutorials in preparation for the training. However, Ubuntu is used in training given the use of PetaLinux. I found the latest PetaLinux Tools Documentation Reference Guide UG1144 (v2019.1) May 22, 2019 which states that Ubuntu Linux 16.04.5, 18.04.1 (64-bit) is the current supported Ubuntu version. I found the version of Ubuntu here: Index of /releases

  • Sign in to reply

Top Comments

  • Fred27
    Fred27 over 7 years ago +1
    I wonder if WSL (Windows Subsystem for Linux) would do the trick? I'm planning to try that soon.
  • buffteethr
    buffteethr over 7 years ago in reply to nerdyupdates +1
    I haven't been able to install the Xilinx tools yet. I spent most of yesterday going through several of the videos. However, installing VM and Ubuntu took about 2 hours. I was having issues installing…
  • nerdyupdates
    nerdyupdates over 7 years ago in reply to buffteethr +1
    Yeah, I agree, it's probably better to stick to the format of the tutorials. Easier to see where something went wrong than doing it a different way. Good to know that's a possibility, though! I have successfully…
Parents
  • nerdyupdates
    nerdyupdates over 7 years ago

    My heart sunk a little when I saw we needed to do all this rather than just install the Xilinx tools on WIndows. Have you had any luck installing the Xilinx tools? I set up the VM and everything seems fine, but I haven't been able to set up the tools. The Xilinx SDx .tar.gz file gets corrupted somehow when copying from the VM shared folder to the VM desktop. There is no error when copying to the desktop, but when extracting and/or running md5sum on the file once on the desktop, I get Input/output error and it fails to extract and/or perform the md5sum. When I run m5sum on the file in the shared folder, it eventually reports the same value Xilinx provides, so I know something is wrong with copying it from the shared folder to the desktop.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dcsoutherner
    dcsoutherner over 7 years ago in reply to nerdyupdates

    The petalinux tools will be needed to get through the builds and installs, so I found you will have to have a linux environment for that.  I haven't looked into a workaround.

    The installation of the Xilinx tools on windows also replaces the "cmd" command utility.  This isn't a big deal (use the Windows TShell utility instead), but I have heartburn over Xilinx replacing a windows component.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Fred27
    Fred27 over 7 years ago in reply to dcsoutherner

    Are you sure that the Xilinx tools replace cmd? I've installed them and I'm pretty sure they don't. It would be a very strange thing to do too. (I must admit I haven't done anything Petalinux specific though.)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Fred27
    Fred27 over 7 years ago in reply to dcsoutherner

    Are you sure that the Xilinx tools replace cmd? I've installed them and I'm pretty sure they don't. It would be a very strange thing to do too. (I must admit I haven't done anything Petalinux specific though.)