Path II Programmable
  • Challenges & Projects
  • Design Challenges
  • Path II Programmable
  • More
  • Cancel
Path II Programmable
Blog Install an Ubuntu Virtual Machine
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
  • Author Author: buffteethr
  • Date Created: 13 Oct 2019 7:54 PM Date Created
  • Views 1610 views
  • Likes 3 likes
  • Comments 8 comments
Related
Recommended

Install an Ubuntu Virtual Machine

buffteethr
buffteethr
13 Oct 2019

I installed the Vivado tools in Windows when I went through other tutorials in preparation for the training. However, Ubuntu is used in training given the use of PetaLinux. I found the latest PetaLinux Tools Documentation Reference Guide UG1144 (v2019.1) May 22, 2019 which states that Ubuntu Linux 16.04.5, 18.04.1 (64-bit) is the current supported Ubuntu version. I found the version of Ubuntu here: Index of /releases

  • Sign in to reply

Top Comments

  • Fred27
    Fred27 over 7 years ago +1
    I wonder if WSL (Windows Subsystem for Linux) would do the trick? I'm planning to try that soon.
  • buffteethr
    buffteethr over 7 years ago in reply to nerdyupdates +1
    I haven't been able to install the Xilinx tools yet. I spent most of yesterday going through several of the videos. However, installing VM and Ubuntu took about 2 hours. I was having issues installing…
  • nerdyupdates
    nerdyupdates over 7 years ago in reply to buffteethr +1
    Yeah, I agree, it's probably better to stick to the format of the tutorials. Easier to see where something went wrong than doing it a different way. Good to know that's a possibility, though! I have successfully…
Parents
  • Fred27
    Fred27 over 7 years ago

    I wonder if WSL (Windows Subsystem for Linux) would do the trick? I'm planning to try that soon.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 7 years ago in reply to Fred27

    It could work unless you get into Linux internals. It is Linux like just as wine is Windows like.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • clem57
    clem57 over 7 years ago in reply to Fred27

    It could work unless you get into Linux internals. It is Linux like just as wine is Windows like.