Path II Programmable
  • Challenges & Projects
  • Design Challenges
  • Path II Programmable
  • More
  • Cancel
Path II Programmable
Forum PIIP - PetaLinux 2018.3 Installation missing files
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 5 subscribers
  • Views 1779 views
  • Users 0 members are here
  • path ii programmable
Related

PIIP - PetaLinux 2018.3 Installation missing files

ralphjy
ralphjy over 6 years ago

Hi,

 

This is a question for my fellow trainees.  I just discovered that I'm missing some files from my PetaLinux install and I just wanted to ask whether others are having this problem or if I have made an error installing or am using a corrupt install.

 

I normally run the SDK from the shortcut icon on my VM desktop and that has been working fine.  In PetaLinux Lab 4 the SDK is started from the command line - xsdk and that failed because it couldn't find the Java runtime required by the SDK (it was a warning but it failed to start).  When PetaLinux was installed the instructions were to modify the .bashrc file so that the PATH was changed to point to the PetaLinux install files.  The JRE files are missing from my PetaLinux file tree (/tools/petalinux-v2018.3-final) but are there for the Xilinx file tree (/tools/Xilinx).

 

I copied files to eliminate the jre problem but encountered more missing files.

 

Anyone else have this problem?  If not I'll have to hunt for why I am missing files.

 

Thanks,

 

Ralph

  • Sign in to reply
  • Cancel
Parents
  • aspork42
    aspork42 over 6 years ago

    Which labs is that for? I tried launching SDK from command line and it didn't work, but the desktop shortcut worked fine with no ill side effects that i've noticed. I've done labs 1-4 and am finishing tonight.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • aspork42
    aspork42 over 6 years ago

    Which labs is that for? I tried launching SDK from command line and it didn't work, but the desktop shortcut worked fine with no ill side effects that i've noticed. I've done labs 1-4 and am finishing tonight.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • ralphjy
    ralphjy over 6 years ago in reply to aspork42

    Thanks, I guess I was looking for confirmation that starting the SDK from the command line did not work.  You probably have the same issue.