Path to Programmable 3
  • Challenges & Projects
  • Design Challenges
  • Path to Programmable 3
  • More
  • Cancel
Path to Programmable 3
Forum Help with XADC Minized ports for ADC External Multiplexer
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Path to Programmable 3 to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 128 subscribers
  • Views 1936 views
  • Users 0 members are here
  • zynq
  • arduino shield
  • amd
  • xadc
  • minized
Related

Help with XADC Minized ports for ADC External Multiplexer

javagoza
javagoza over 3 years ago

I'm planning to design an external ADC 16:2 multiplexer board for the two channel 12-bit 1MSPS ADC on the XADC Minized Zynq

image


I have seen in the schematic that I can access the AD0P, AD0N, AD8P and AD8N ports from the headers for the Arduino Shield, the pins ARDUINO_A2, ARDUINO_A3, ARDUINO_A4, ARDUINO_A5
The ARDUINO_A2 pin is only connected to the Zynq Bank 35 but

  • ARDUINO_A3 and ARDUINO_A4 are both connected to the gate of two BSS138 N-CHANNEL MOSFET for controlling the bi-element PL-LED. As I will use both input channels as unipolar those pins will be connected to GND.
  • The ARDUINO_A5 is connected to the DIP PL switch, so I think I can switch off that switch.

My question is if what I'm thinking is safe and can I use those ports with that configuration?

  • ARDUINO_A3 -> GND
  • ARDUINO_A4 -> GND
  • SW1 -> OFF -> GND

image

  • Sign in to reply
  • Cancel

Top Replies

  • javagoza
    javagoza over 3 years ago +2
    This is what I planning to build:
  • michaelkellett
    michaelkellett over 3 years ago in reply to javagoza +2
    It looks OK to me but rather than grounding the pins directly why not link them to ground by 470R or so and test. If no volts across 470R you can short them if the ADC is noisy. If you ground them…
  • javagoza
    javagoza over 3 years ago in reply to javagoza +1
    Just published the blog! community.element14.com/.../p2p3-amd-zynq-7000-soc-xadc-external-multiplexer-mode
  • javagoza
    0 javagoza over 3 years ago

    This is what I planning to build:

    image

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 3 years ago in reply to javagoza

    It looks OK to me but rather than grounding the pins directly why not link them to ground by 470R or so and test.

    If no volts across 470R you can short them if the ADC is noisy.

    If you ground them and run an image on the FPGA that pulls them high you might blow a pin driver .

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • javagoza
    0 javagoza over 3 years ago in reply to michaelkellett

    Thank you very much Michael! I will follow your advice, better safe than sorry. I will post the results in a future blog.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • javagoza
    0 javagoza over 3 years ago in reply to javagoza

    Just published the blog!

     

    P2P3 AMD Zynq-7000 SoC XADC. External Multiplexer Mode.
    javagoza
    P2P3 AMD Zynq-7000 SoC XADC. External Multiplexer Mode.
    The Avnet Minized board only exposes 4 channels of…
    By javagoza over 3 years ago in Path to Programmable 3 > Blog
    4 comments