Path to Programmable 3
  • Challenges & Projects
  • Design Challenges
  • Path to Programmable 3
  • More
  • Cancel
Path to Programmable 3
Forum Need a boot manager for dual boot windows 11 and Ubuntu
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Path to Programmable 3 to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 130 subscribers
  • Views 4152 views
  • Users 0 members are here
  • petalinux
  • ultra96
  • Path Programmable III
  • installation
Related

Need a boot manager for dual boot windows 11 and Ubuntu

manojroy123
manojroy123 over 3 years ago

I am looking for an UEFI boot manager for setting up dual boot operating system. my operating system will be windows 11 and ubuntu/Redhat. windows boot manager is not working properly. Can some one suggest good UEFI boot manager for the above applications

  • Sign in to reply
  • Cancel

Top Replies

  • Gough Lui
    Gough Lui over 3 years ago +1
    Why don't you use the preferred one by most Linux distributions - GRUB? It's usually installed by default if you install Linux after Windows ... and usually works just fine. Perhaps you have some strange…
  • Gough Lui
    Gough Lui over 3 years ago

    Why don't you use the preferred one by most Linux distributions - GRUB? It's usually installed by default if you install Linux after Windows ... and usually works just fine.

    Perhaps you have some strange UEFI/Secure Boot requirements for full disk encryption (e.g. Bitlocker) that is causing problems?

    - Gough

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • ggabe
    ggabe over 3 years ago

    Have you thought about VMware Workstation Player instead of dual boot?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Fred27
    Fred27 over 3 years ago

    I seconds Gough Lui's suggestion of using GRUB. If you install Windows for and then Linux it should be fairly seamless.

    However, it's been a long time since I used dual boot. Unless you really need to, it's often more trouble than it's worth. There are other options like virtualization, Docker, WSL2 that may work well - depending on your requirements.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • manojroy123
    manojroy123 over 3 years ago

    I tried everything almost for past 10 to 15 days to create dual boot device but failed in my effort to create it.