Path to Programmable
  • Challenges & Projects
  • Design Challenges
  • Path to Programmable
  • More
  • Cancel
Path to Programmable
Blog Day 0 - MiniZed ZYNQ FPGA Arrives
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
  • Author Author: snidhi
  • Date Created: 7 Oct 2018 12:13 PM Date Created
  • Views 1500 views
  • Likes 5 likes
  • Comments 6 comments
  • fpga
  • avnet minized
  • fpga developement
  • minized
Related
Recommended

Day 0 - MiniZed ZYNQ FPGA Arrives

snidhi
snidhi
7 Oct 2018

Last Thursday I finally received the MiniZed development board from Element14. Many thanks to the community and the element14 judges for selecting me as one of the participants.

The development board was well packed and came in with some essential info on to-dos and don'ts with the MiniZed board. A humble USB cable for powering and some jumpers if needed I would guess.

 

As advertised the MiniZed ZYNQ kit should include the following things in the box

image

 

The Unboxing and Test

 

image

image

image

image

 

Powering on the MiniZed. All the LEDS look good to go.

image

image

As one can see on the reverse side the board has no support legs but mini rubber pads for sitting on the table. Although it has oddly placed 3 mounting holes from what it looks like (somehow not 4 mounting holes image). For what purpose are these holes other than decorative no idea yet image I am pretty sure these three not so equally placed holes will be able to support the board on its own.

 

As everyone else I have already received the training material for the MiniZed board as well from Xilinx.

 

And currently I am dedicating some time to go through the training material and do first programming with the MiniZED board.

  • Sign in to reply

Top Comments

  • Gough Lui
    Gough Lui over 8 years ago +3
    Nice to see the board up-close. Quite a packed board indeed. It seems like the three holes are in the same place as the holes on the Arduino Uno-type boards - it's probably for compatibility reasons with…
  • snidhi
    snidhi over 8 years ago in reply to Gough Lui +3
    yes, the board is pretty tightly made. I have seen recently many of the FPGA dev-boards are coming without any mounting holes. I personally prefer them but of-course it adds to the pcb size. But they can…
  • genebren
    genebren over 8 years ago +3
    Nice looking board indeed. Good luck on your training exercises and the successful completion of your project! Gene
  • snidhi
    snidhi over 8 years ago in reply to shabaz

    Good luck to you as well.

    I think the holes are for mounting arduino compatible sensor-hats

     

    Cheers

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 8 years ago

    Hehe I couldn't understand the hole strategy either.

    As for the jumpers.. maybe they fell off a different production line : ) mine didn't have them (although I should double-check now! : )

    Good luck with the course!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • snidhi
    snidhi over 8 years ago in reply to genebren

    Thanks Gene image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 8 years ago

    Nice looking board indeed.  Good luck on your training exercises and the successful completion of your project!

    Gene

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • snidhi
    snidhi over 8 years ago in reply to Gough Lui

    yes, the board is pretty tightly made. 

     

    I have seen recently many of the FPGA dev-boards are coming without any mounting holes. I personally prefer them but of-course it adds to the pcb size. But they can be then fixed on some mechanical frame or casing.

     

    I guess glue gun is the only temporary solution. image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
>