Path to Programmable
  • Challenges & Projects
  • Design Challenges
  • Path to Programmable
  • More
  • Cancel
Path to Programmable
Blog I'm back! And I got Vivado installed :)
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
  • Author Author: aspork42
  • Date Created: 19 Oct 2018 8:02 PM Date Created
  • Views 1210 views
  • Likes 7 likes
  • Comments 2 comments
  • soc
  • avnet
  • path to programmable
  • xilinx
  • fpga
Related
Recommended

I'm back! And I got Vivado installed :)

aspork42
aspork42
19 Oct 2018

Well I had to spend a week on-site with a customer and another week at a trade show; but I'm back!

 

I'm happy to report that I got Vivado 2017.4 installed. I followed the instructions in this "experiment" to install the dev environment... although I was a little worried why Xilinx considers installing software an experiment...

image

 

I started by creating an account on the Xilinx website. It was a little tricky since they don't trust the apostrophe in my last name... The story of my life...

 

image

 

And for some reason, even the US Government gets involved and they didn't like it either.

image

 

At least if they ever try to find James Ogorman, then they'll never find me image

 

Lab 0 is just about downloading and installing and it overall goes pretty quick.

 

There are also some accompanying videos for each lesson. We are doing Hardware training (as opposed to the available software training package) so the first video is an introduction to the hardware.

I learned about how the SoC (System On Chip) is a combined FPGA and ARM Processor. This gives it the benefit of hardware-based speed for recurring tasks like video stream processing and an ARM processor which can run a full-blown operating system like Linux; all in one. This also can mean lower overall power consumption on a device since it is a single chip and they are also advertising this as a less hackable piece of hardware since it is all in one.

 

I'm on to the next lesson but wanted to get this quick post out there so I don't fall too far behind on this quick training program!

  • Sign in to reply

Top Comments

  • DAB
    DAB over 7 years ago +3
    Nice to have you back. Missing two weeks puts you behind the others, but you can probably make up time if things go well and you are a quick learner. DAB
  • genebren
    genebren over 7 years ago +2
    Good to have you back on the path. Hopefully you will not have too much trouble catching up with the others. Gene
Parents
  • genebren
    genebren over 7 years ago

    Good to have you back on the path.  Hopefully you will not have too much trouble catching up with the others.

     

    Gene

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • genebren
    genebren over 7 years ago

    Good to have you back on the path.  Hopefully you will not have too much trouble catching up with the others.

     

    Gene