Path to Programmable
  • Challenges & Projects
  • Design Challenges
  • Path to Programmable
  • More
  • Cancel
Path to Programmable
Blog Path to Programmable - Blog 10 - Video Project
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
  • Author Author: rsc
  • Date Created: 6 Jan 2019 4:26 AM Date Created
  • Views 1047 views
  • Likes 3 likes
  • Comments 5 comments
  • path to programmable
  • minized
Related
Recommended

Path to Programmable - Blog 10 - Video Project

rsc
rsc
6 Jan 2019

My project is to do something interesting with the PMOD TDM114 camera module.

I found a demo project on the Avnet site called "MJPEG Video Streaming on Avnet MiniZed"

It looks like exactly what I needed to start this project, so I downloaded the quick start guide.

The first thing to do was Flash the boot image boot_QSPI.bin to QSPI.  There is a command line tool for this in the SDK package.

image

image

I used the hardware platform and First Stage Boot Loader (fsbl) from the ZynqSW labs and it flashed ok.

image

Then I transferred the image files from a USB drive to the eMMC.

I had some issues with the demo quick start guide on where my USB drive was mounted, but I figured it out and transferred the files OK

image

Then I needed to Flash the boot image smallboot.bin to QSPI using the SDK

image

The next task was to navigate to the demo application location and start it.

# cd /run/media/mmcblk1p1/mjpeg_demo

# ./run.sh

image

Success!

The image is a bit dark, but it's streaming.  Now to dig into the demo code and see what I can do with it.

  • Sign in to reply

Top Comments

  • rscasny
    rscasny over 7 years ago +1
    I like the camera idea. Randall
Parents
  • genebren
    genebren over 7 years ago

    Nice update!  Is the green tinting in the image an artifact of the camera and/or logic, or just part of the overall dark image? 

     

    Gene

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • genebren
    genebren over 7 years ago

    Nice update!  Is the green tinting in the image an artifact of the camera and/or logic, or just part of the overall dark image? 

     

    Gene