Path to Programmable
  • Challenges & Projects
  • Design Challenges
  • Path to Programmable
  • More
  • Cancel
Path to Programmable
Blog SW Module 4
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
  • Author Author: mconners
  • Date Created: 16 Dec 2018 1:03 PM Date Created
  • Views 960 views
  • Likes 4 likes
  • Comments 2 comments
Related
Recommended

SW Module 4

mconners
mconners
16 Dec 2018

This lab was mostly more familiarization with the SDK.

 

The lab goals were stated as follows:

 

Add new software applications to SDK

Use example code to target the UART in a Hello World application

Apply example project templates, including

      Memory Tests

      Peripheral Tests

Identify application code size and location

Modify linker scripts to change the target memory location

 

So we started out by creating an empty application, then bringing in source from the examples linked in the Board Support Package that we generated in the previous lab.We then looked at the output of the compilation,

the types of files generated, an the size of the file generated.

 

We took a look at the linker script, lscript.ld, this is the file that contains all of the memory mapping for the project, and this is always chip specific. I remember a few years ago, when I was first starting out programming arm chips, this file,

which is essential was very difficult to find for many chips, so you would have to make it on your own, often wrong.

 

/*******************************************************************/
/*                                                                 */
/* This file is automatically generated by linker script generator.*/
/*                                                                 */
/* Version:                                 */
/*                                                                 */
/* Copyright (c) 2010-2016 Xilinx, Inc.  All rights reserved.      */
/*                                                                 */
/* Description : Cortex-A9 Linker Script                          */
/*                                                                 */
/*******************************************************************/


_STACK_SIZE = DEFINED(_STACK_SIZE) ? _STACK_SIZE : 0x2000;
_HEAP_SIZE = DEFINED(_HEAP_SIZE) ? _HEAP_SIZE : 0x0;


_ABORT_STACK_SIZE = DEFINED(_ABORT_STACK_SIZE) ? _ABORT_STACK_SIZE : 1024;
_SUPERVISOR_STACK_SIZE = DEFINED(_SUPERVISOR_STACK_SIZE) ? _SUPERVISOR_STACK_SIZE : 2048;
_IRQ_STACK_SIZE = DEFINED(_IRQ_STACK_SIZE) ? _IRQ_STACK_SIZE : 1024;
_FIQ_STACK_SIZE = DEFINED(_FIQ_STACK_SIZE) ? _FIQ_STACK_SIZE : 1024;
_UNDEF_STACK_SIZE = DEFINED(_UNDEF_STACK_SIZE) ? _UNDEF_STACK_SIZE : 1024;


/* Define Memories in the system */


MEMORY
{
   axi_bram_ctrl_0_Mem0 : ORIGIN = 0x40000000, LENGTH = 0x2000
   ps7_ddr_0 : ORIGIN = 0x100000, LENGTH = 0x1FF00000
   ps7_qspi_linear_0 : ORIGIN = 0xFC000000, LENGTH = 0x1000000
   ps7_ram_0 : ORIGIN = 0x0, LENGTH = 0x30000
   ps7_ram_1 : ORIGIN = 0xFFFF0000, LENGTH = 0xFE00
}


/* Specify the default entry point to the program */


ENTRY(_vector_table)


/* Define the sections, and where they are mapped in memory */


SECTIONS
{
.text : {
   KEEP (*(.vectors))
   *(.boot)
   *(.text)
   *(.text.*)
   *(.gnu.linkonce.t.*)
   *(.plt)
   *(.gnu_warning)
   *(.gcc_execpt_table)
   *(.glue_7)
   *(.glue_7t)
   *(.vfp11_veneer)
   *(.ARM.extab)
   *(.gnu.linkonce.armextab.*)
} > ps7_ram_0


.init : {
   KEEP (*(.init))
} > ps7_ram_0


.fini : {
   KEEP (*(.fini))
} > ps7_ram_0


.rodata : {
   __rodata_start = .;
   *(.rodata)
   *(.rodata.*)
   *(.gnu.linkonce.r.*)
   __rodata_end = .;
} > ps7_ram_0


.rodata1 : {
   __rodata1_start = .;
   *(.rodata1)
   *(.rodata1.*)
   __rodata1_end = .;
} > ps7_ram_0


.sdata2 : {
   __sdata2_start = .;
   *(.sdata2)
   *(.sdata2.*)
   *(.gnu.linkonce.s2.*)
   __sdata2_end = .;
} > ps7_ram_0


.sbss2 : {
   __sbss2_start = .;
   *(.sbss2)
   *(.sbss2.*)
   *(.gnu.linkonce.sb2.*)
   __sbss2_end = .;
} > ps7_ram_0


.data : {
   __data_start = .;
   *(.data)
   *(.data.*)
   *(.gnu.linkonce.d.*)
   *(.jcr)
   *(.got)
   *(.got.plt)
   __data_end = .;
} > ps7_ram_0


.data1 : {
   __data1_start = .;
   *(.data1)
   *(.data1.*)
   __data1_end = .;
} > ps7_ram_0


.got : {
   *(.got)
} > ps7_ram_0


.ctors : {
   __CTOR_LIST__ = .;
   ___CTORS_LIST___ = .;
   KEEP (*crtbegin.o(.ctors))
   KEEP (*(EXCLUDE_FILE(*crtend.o) .ctors))
   KEEP (*(SORT(.ctors.*)))
   KEEP (*(.ctors))
   __CTOR_END__ = .;
   ___CTORS_END___ = .;
} > ps7_ram_0


.dtors : {
   __DTOR_LIST__ = .;
   ___DTORS_LIST___ = .;
   KEEP (*crtbegin.o(.dtors))
   KEEP (*(EXCLUDE_FILE(*crtend.o) .dtors))
   KEEP (*(SORT(.dtors.*)))
   KEEP (*(.dtors))
   __DTOR_END__ = .;
   ___DTORS_END___ = .;
} > ps7_ram_0


.fixup : {
   __fixup_start = .;
   *(.fixup)
   __fixup_end = .;
} > ps7_ram_0


.eh_frame : {
   *(.eh_frame)
} > ps7_ram_0


.eh_framehdr : {
   __eh_framehdr_start = .;
   *(.eh_framehdr)
   __eh_framehdr_end = .;
} > ps7_ram_0


.gcc_except_table : {
   *(.gcc_except_table)
} > ps7_ram_0


.mmu_tbl (ALIGN(16384)) : {
   __mmu_tbl_start = .;
   *(.mmu_tbl)
   __mmu_tbl_end = .;
} > ps7_ram_0


.ARM.exidx : {
   __exidx_start = .;
   *(.ARM.exidx*)
   *(.gnu.linkonce.armexidix.*.*)
   __exidx_end = .;
} > ps7_ram_0


.preinit_array : {
   __preinit_array_start = .;
   KEEP (*(SORT(.preinit_array.*)))
   KEEP (*(.preinit_array))
   __preinit_array_end = .;
} > ps7_ram_0


.init_array : {
   __init_array_start = .;
   KEEP (*(SORT(.init_array.*)))
   KEEP (*(.init_array))
   __init_array_end = .;
} > ps7_ram_0


.fini_array : {
   __fini_array_start = .;
   KEEP (*(SORT(.fini_array.*)))
   KEEP (*(.fini_array))
   __fini_array_end = .;
} > ps7_ram_0


.ARM.attributes : {
   __ARM.attributes_start = .;
   *(.ARM.attributes)
   __ARM.attributes_end = .;
} > ps7_ram_0


.sdata : {
   __sdata_start = .;
   *(.sdata)
   *(.sdata.*)
   *(.gnu.linkonce.s.*)
   __sdata_end = .;
} > ps7_ram_0


.sbss (NOLOAD) : {
   __sbss_start = .;
   *(.sbss)
   *(.sbss.*)
   *(.gnu.linkonce.sb.*)
   __sbss_end = .;
} > ps7_ram_0


.tdata : {
   __tdata_start = .;
   *(.tdata)
   *(.tdata.*)
   *(.gnu.linkonce.td.*)
   __tdata_end = .;
} > ps7_ram_0


.tbss : {
   __tbss_start = .;
   *(.tbss)
   *(.tbss.*)
   *(.gnu.linkonce.tb.*)
   __tbss_end = .;
} > ps7_ram_0


.bss (NOLOAD) : {
   __bss_start = .;
   *(.bss)
   *(.bss.*)
   *(.gnu.linkonce.b.*)
   *(COMMON)
   __bss_end = .;
} > ps7_ram_0


_SDA_BASE_ = __sdata_start + ((__sbss_end - __sdata_start) / 2 );


_SDA2_BASE_ = __sdata2_start + ((__sbss2_end - __sdata2_start) / 2 );


/* Generate Stack and Heap definitions */


.heap (NOLOAD) : {
   . = ALIGN(16);
   _heap = .;
   HeapBase = .;
   _heap_start = .;
   . += _HEAP_SIZE;
   _heap_end = .;
   HeapLimit = .;
} > ps7_ram_0


.stack (NOLOAD) : {
   . = ALIGN(16);
   _stack_end = .;
   . += _STACK_SIZE;
   . = ALIGN(16);
   _stack = .;
   __stack = _stack;
   . = ALIGN(16);
   _irq_stack_end = .;
   . += _IRQ_STACK_SIZE;
   . = ALIGN(16);
   __irq_stack = .;
   _supervisor_stack_end = .;
   . += _SUPERVISOR_STACK_SIZE;
   . = ALIGN(16);
   __supervisor_stack = .;
   _abort_stack_end = .;
   . += _ABORT_STACK_SIZE;
   . = ALIGN(16);
   __abort_stack = .;
   _fiq_stack_end = .;
   . += _FIQ_STACK_SIZE;
   . = ALIGN(16);
   __fiq_stack = .;
   _undef_stack_end = .;
   . += _UNDEF_STACK_SIZE;
   . = ALIGN(16);
   __undef_stack = .;
} > ps7_ram_0


_end = .;
}

The main purpose of the linker script is to describe how the sections in the input files should be mapped

into the output file, and to control the memory layout of the output file.

 

The second experiment was to add peripheral tests and study the files included. We had built this project as part of the hardware labs as well. This was a more thorough inspection of the generated files.

 

The third experiment was the memory test example, like the peripheral test, this was one we did in the HW module, we just went in and looked at the files and examined what would happen in we moved some of the memory regions around.

 

Oddly, we did not execute any of these examples on the board. It will be interesting to see what lab 5 brings.

 

See you then.

  • Sign in to reply

Top Comments

  • mconners
    mconners over 7 years ago in reply to DAB +1
    LOL! Hey, DAB. Oh, they compile, and honestly, they were the same examples that we did in the HW labs. So, I've actually copied and pasted the outputs in the other labs. They just explained a bit more…
  • mconners
    mconners over 7 years ago in reply to DAB

    LOL!

     

    Hey, DAB. Oh, they compile, and honestly, they were the same examples that we did in the HW labs. So, I've actually copied and pasted the outputs in the other labs.

     

    They just explained a bit more in these. I started looking at Lab 5 today, and this one they definitely have us programming the board :-)

     

     

    Mike

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 7 years ago

    You might try the examples just to see if they compile.

     

    I agree, it is odd that they did not have you run the examples on the board.

     

    I wonder what they might be hiding.

     

    DAB