Products
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
Path to Programmable
  • Challenges & Projects
  • Design Challenges
  • Path to Programmable
  • More
  • Cancel
Path to Programmable
Forum SDK with Windows 10 problem
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 5 subscribers
  • Views 1321 views
  • Users 0 members are here
  • xilinx sdk
Related

SDK with Windows 10 problem

rsc
rsc over 7 years ago

I've been having a problem with the SDK while trying to complete the labs.  When I start a new application and select one of the templates such as Hello World, the SDK closes after it makes the directories.  I have to restart the SDK to download and run.  Is anyone else having this problem? It doesn't happen every time though, sometimes it just minimizes the SDK window while it's compiling.

 

Scott

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 7 years ago +1
    Hi Scott, I've not seen that yet, but I've only created one application based on the template. I'll try tonight to create several more applications, in an attempt to replicate what you're seeing. I'm running…
  • rsc
    rsc over 7 years ago in reply to shabaz +1
    I'll look at that next time, Vivado takes 26 seconds to start up also, have you seen that? I wonder if this PC is having page faults or swap issues. It looks like my CPU usage goes to %100 when the SDK…
  • Fred27
    Fred27 over 7 years ago in reply to rsc +1
    It's painfully slow to open, isn't it? And not even a splash screen whilst you wait to show that you have done it. It also seems strange that it takes ages to synthesize a design compared to compiling…
Parents
  • snidhi
    snidhi over 7 years ago

    I had the issue that sometimes when I launched the SDK from Vivado the SDK folder would be made and then suddenly SDK shut down automatically without a warning.

     

    I refreshed and restarted the SDK standalone and just went ahead with the recent design file. I am also using Windows 10

     

    Cheers

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • snidhi
    snidhi over 7 years ago

    I had the issue that sometimes when I launched the SDK from Vivado the SDK folder would be made and then suddenly SDK shut down automatically without a warning.

     

    I refreshed and restarted the SDK standalone and just went ahead with the recent design file. I am also using Windows 10

     

    Cheers