• Products and Partners
    Products and Partners
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
Pi IoT
  • Challenges & Projects
  • Design Challenges
  • Pi IoT
  • More
  • Cancel
Pi IoT
Blog 3D Printed Mounting Stand for Raspberry Pi 7'' Display
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
  • Author Author: carmelito
  • Date Created: 20 Jun 2016 4:11 AM Date Created
  • Views 1166 views
  • Likes 6 likes
  • Comments 1 comment
  • 3dprint
  • picontrolhub
  • piiot
  • 3D Printing
  • piiot challenge
Related
Recommended

3D Printed Mounting Stand for Raspberry Pi 7'' Display

carmelito
carmelito
20 Jun 2016

After receiving my package on Friday evening and unboxing all the Raspberry Pi goodies in the element14 brown box .. And after being overcome by happiness image ! looking at the awesome Pi 7" display , I knew the first thing that I had to do was to 3D print a holder/Stand for the screen.

 

So , here you go !! download the 3 STL files attached and 3D print yourself a stand for your Pi 7" screen. The STL file (PlacardPiIOT.stl) is optional which connects the two legs.

And connected at the back of the display is Raspberry Pi B+ .To attach the legs of the stand to the Pi Display you will need 4-40x3/8 screws that you can get at your local hardware store.

 

{gallery:width=900,height=400,autoplay=true} 3D Printed Stand for Pi Display

image

Front: 3D printed stand

image

Top: Power and audio jack connected from the top

image

Legs after 3D Printing: to attach the legs to the stand you will need 4-40x3/8 screws

image

Back: Display connected to a Raspberry Pi B+

 

All the part above where printed in 1.75 mm PLA and here are some suggested setting silcer settings

  • Layer height for the legs:0.3 mm
  • Infill: 20%
  • Temperature : 205 C (i am using Hatchbox filament, please check you filament manufacture site for your filament  )
  • Printing the 3 Stl files took be about 50 mins..
  • To paint the letter, you can use Uni Paint markers

 

 

Now, once you have loaded the SD card with the latest version of Raspbian Jessie , you will observe that the OS/Desktop loads up side down, with the setup as shown in the pictures above. Basically, you can turn the display image,but I found that adding the power cable and audio cable from the top makes it much easier, as shown in the pictures above.

 

Now to solve the upside-down issue you need to add the following line to the config.txt file, if you have a wireless keyboard connected open the terminal and run the following command

 

sudo nano /boot/config.txt

 

and then add the following line to the file

lcd_rotate=2

 

image

 

At this point, I would like to take a moment to thank element14 for sending out the awesome hardware for PiIoT challenge ...

Attachments:
STLsPi7inScreenStand.zip
  • Sign in to reply
Parents
  • carmelito
    carmelito over 10 years ago

    You can also find the STL files at

    http://www.thingiverse.com/thing:1664964

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • carmelito
    carmelito over 10 years ago

    You can also find the STL files at

    http://www.thingiverse.com/thing:1664964