Pi IoT
  • Challenges & Projects
  • Design Challenges
  • Pi IoT
  • More
  • Cancel
Pi IoT
Blog IoT Farm: Blog 12 - Farm Eyes, Success!
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
  • Author Author: jkutzsch
  • Date Created: 29 Aug 2016 4:22 AM Date Created
  • Views 916 views
  • Likes 4 likes
  • Comments 3 comments
  • pi iot
  • farm
  • farm_technology
  • pi iot design challenge
Related
Recommended

IoT Farm: Blog 12 - Farm Eyes, Success!

jkutzsch
jkutzsch
29 Aug 2016

In previous blogs i had shared my issues of having the RPi B+ running MotionEyeOs with multiple cameras and wireless networking enabled.

 

Today I have had success getting everything outside and monitoring the Farm!

 

First off, hardwired I have had zero issues with the MotionEyeOs software.  I have been able to add cameras and test everything out without any issues other then the RPi B+ is (not surprisingly) noticeably slower for response then the RPi3 that I first used.

 

But once I attempted to go enable WiFi I constantly ran into issues.  Finally after creating a brand new image, ensuring all of the WiFi credential information was correct and running off the same AP for all of my communications I was able to get WiFi running last night.  Things were looking good.

 

But today when I had reassembled all of my gear and installed it outside I was not able to connect.

 

After verifying power and all connections I could watch the RPi B+ boot up and the WiPi flash but when I tried to connect to the static IP, no luck.  After pulling off the extra cameras and trying it just as a base system and still having no luck I decided to completely bring everything back inside and retry it there.

 

Success!  Right away I was connected again via Wireless and able to see all 3 cameras.

 

Doing a little research on others experience with the WiPi made it sound like some people had issues with some of the dongles having limited range.  Very limited range.

 

This had not been factored into my planning since I have my AP at an outside window and pretty much all of our electronics have been successful connecting from the outside and streaming the kids various flavor of entertainment at that moment.  Youtube, Spotify, Netflix, it all was useable.

 

Luckily I had a Realtek wireless dongle and I swapped that in for the WiPi and everything was working again.  Outside!

 

MotionEyeOs even automatically adjusted for the different card and I was able to both ping the RPi B+ and connect into the monitoring software.

 

image

 

Camera 1 is the baby box monitor, currently looking at the rear of the Momma Rabbit.  As of today, no babies, but they are expected soon.

Camera 2 is the front of the Momma Rabbits cage, usually she is right there checking things out, but right now she is trying to figure out what that camera is doing in her box.  :-)

Camera 3 is the View to the Chicken Casa.

 

image

 

Here in Camera 1 we can see Momma's Ear, she had just put her eye right up to the camera checking everything out.

 

image

 

Here is Momma starting to get a little concerned from all of the camera's and activity.

 

image

 

Here I tried to zoom externally on the Chicken Casa Camera, hard to tell but there is a variety of Chickens and G.O.A.Ts scrambling for treats.  The image is a lot easier to see on screen then it is when captured.

 

image

 

Here is a close up of the Baby Box, I put a block of wood in the corner as a focal point.

 

I quickly shutdown all of the activity around the Rabbits and Monitoring Station to allow Momma to get used to everything.  I think I may move Camera 2 over to monitor another part of the Farm and allow for just Camera 1 to watch the Baby Box.  Letting her get used to everything.

 

 

 

image

 

I really like the functionality of the Cameras and will be ordering some more to see about combining cameras to get a broader range of monitoring.  I used a clear snack box as a cover for the USB Cameras and it functioned very well.  I wanted to add more weather proofing then just having the cameras under a shelter roof.

 

image

 

Yes, I like the way the whole setup is working now and look forward to adding/improving upon it!

 

 

And as a final picture, here is a test run of the efforts of my son and I for making a larger Duck Pond.  I wanted to see how level everything is and how long the water naturally stays in our heavy clay area.

image

 

Eventually a little bridge will be added over that middle giving the ducks more shade to work with and the kids something neat to walk across and see their ducklings.

  • Sign in to reply

Top Comments

  • DAB
    DAB over 10 years ago +1
    Ah yes, never a dull moment on the farm. It looks like you have your initial system in place. I am sure refinements will be needed over time, but you have the basis for a reasonable monitoring system.…
  • jkutzsch
    jkutzsch over 10 years ago in reply to DAB +1
    Yes, definitely more refinements already planned! More cameras, better locations, and of course sensor tie ins. Oddly enough I tried to post my last to blogs to the IoT design Challenge but I couldn't…
Parents
  • DAB
    DAB over 10 years ago

    Ah yes, never a dull moment on the farm.

     

    It looks like you have your initial system in place.

     

    I am sure refinements will be needed over time, but you have the basis for a reasonable monitoring system.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jkutzsch
    jkutzsch over 10 years ago in reply to DAB

    Yes, definitely more refinements already planned!  More cameras, better locations, and of course sensor tie ins.  Oddly enough I tried to post my last to blogs to the IoT design Challenge but I couldn't seem to find it and had to post them over to just Design Challenge blog. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jkutzsch
    jkutzsch over 10 years ago in reply to jkutzsch

    Strange, I went back later and the site was down for a short period and then I was able to find the IoT blog again for adding information.  So I moved the previous posts over to that more appropriate location.  Makes me wonder if I was just so flustered from not getting some of the hardware working that I missed something in the creation of the blogs.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jkutzsch
    jkutzsch over 10 years ago in reply to jkutzsch

    Strange, I went back later and the site was down for a short period and then I was able to find the IoT blog again for adding information.  So I moved the previous posts over to that more appropriate location.  Makes me wonder if I was just so flustered from not getting some of the hardware working that I missed something in the creation of the blogs.