Pi IoT
  • Challenges & Projects
  • Design Challenges
  • Pi IoT
  • More
  • Cancel
Pi IoT
Blog Pi Control Hub: Integrating Camera's in Home Assistant
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
  • Author Author: carmelito
  • Date Created: 23 Aug 2016 7:05 PM Date Created
  • Views 5170 views
  • Likes 4 likes
  • Comments 6 comments
  • home automation
  • raspberry pi zero
  • piiot
  • raspberry pi3
  • raspberry pi
  • security_camera
  • picamera
  • piiot challenge
Related
Recommended

Pi Control Hub: Integrating Camera's in Home Assistant

carmelito
carmelito
23 Aug 2016

Here is a quick post on integrating camera's with Home Assistant, this includes

  • Pi Camera connected to Raspberry Pi 3 as part of the Hub
  • Security camera that we create using a Raspberry Pi Zero, PI NOIR camera and installing Motion with Single File PHP Gallery in a previous blog post - Pi Control Hub: Spoke 1 :Security Camera

 

Basically, as part of Home Assistant dashboard we are going to add two sections  showing the preview of Pi Cameras as shown in the pictures below

{gallery} Integrating Camera's in Home Assistant

image

Home Assistant dashboard with Pi Cameras preview.

image

Security Camera setup with Pi Zero + NOIR camera, in a 3D printed case.

image

Pi camera connected  to the Raspberry Pi 3

image

Security camera feed in a  separate tab

image

Picture gallery of the intruders detected image , using Single File PHP Gallery

image

Having a close look into the picture from the Picture gallery

 

 

Here are the steps to follow to integrate the Pi cameras with Home-Assistant

#1  Connect the Pi camera to Raspberry Pi 3 and run the following commands to create a directory called picamera

         pi@hub:~ $ cd /home/hass

         pi@hub:~ $sudo mkdir picamera

         pi@hub:/home/hass $ ls

         picamera

         pi@hub:/home/hass $ sudo chown hass picamera

      and then create a image file

        pi@hub:/home/hass/picamera $   touch image.jpg

 

#2 Update the configuration.yaml file

camera:
  platform: rpi_camera
  name: Raspberry Pi Camera
  image_width: 640
  image_height: 480
  image_quality: 7
  image_rotation: 0
  timelapse: 1000
  horizontal_flip: 0
  vertical_flip: 0
  file_path: /home/hass/picamera/image.jpg

   and then stop and start Home-Assistant and test

      sudo systemctl stop home-assistant@hass

      sudo systemctl start home-assistant@hass

image

 

#3 Adding the Security camera  to the dashboard

    modify the configuration.yaml to include the following under the camera section

- platform: mjpeg
  mjpeg_url: http://192.168.0.21:8081
  name: Security Camera

    change the ip address above with the security camera Pi's ip address

 

#4 To add Security camera Preview tab and the Intruder detection tab which show the picture gallery

       Add the following under the panel_iframe section of the configuration.yaml file

  intruder:
    title: 'Intruder detection'
    icon: 'mdi:nature-people'
    url: 'http://192.168.0.21/'
  securitycam:
    title: 'Security Cam'
    icon: 'mdi:camera'
    url: 'http://192.168.0.21:8081/'

      change the ip address above with the security camera Pi's ip address

  • Sign in to reply

Top Comments

  • volly
    volly over 9 years ago +1
    carmelito . nice touch!
  • cortado
    cortado over 6 years ago +1
    Wwhat operating system are you using? I am on Hassio and cannot enable PI camera. Familiar with that?
  • volly
    volly over 9 years ago

    carmelito. nice touch!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<