Pi IoT
  • Challenges & Projects
  • Design Challenges
  • Pi IoT
  • More
  • Cancel
Pi IoT
Blog [Pi IoT] Plant Health Camera #3 - First steps
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
  • Author Author: gpolder
  • Date Created: 2 Jul 2016 5:57 PM Date Created
  • Views 900 views
  • Likes 4 likes
  • Comments 2 comments
  • LEGO
  • piiot
  • pi3
  • piiot challenge
  • 7.0inch display
  • case
Related
Recommended

[Pi IoT] Plant Health Camera #3 - First steps

gpolder
gpolder
2 Jul 2016

This week I did the first steps in getting the project started.

  • Installed Raspbian on the Pi 3
  • connected the 7" Touchscreen display to the Pi

 

Every thing went flawlessly. I mainly did the same steps as rhavourd in ([Pi IoT] Hangar Central #3 -- Unboxing the Challenge Kit), but didn't make such nice video's / blog post.

Just a note on the I2C connections, these are not needed for the Pi 3, since they are in the DSI interface cable.

 

Here are some images of the result:

image

image

 

 

Now I have the Pi 3 running, I need a case, in which also the other Pi and two cameras can be mounted.

I found a very nice one, the Smarti Pi Touch, which also includes a case for the camera, The case includes the popular LEGO compatible camera case that works with the Pi camera. It has  a lego compatible back and can attach to the case on the back lego plate or the front if you choose to have LEGO compatibility on the front. This will make it very suitable for the application.

I have to think about how to connect the second Pi and Camera.

 

I will order this case next week, and try to get an extra camera case for my second camera.

 

imageimageimage

 

stay tuned!

  • Sign in to reply
Parents
  • DAB
    DAB over 10 years ago

    Nice build for the RPi 3 an camera.

     

    Yes, I have been wondering how you are going to add a second camera.

     

    It might be easier to just use a second RPi and network them together.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • gpolder
    gpolder over 10 years ago in reply to DAB

    That was exactly the idea,

     

    Gerrit.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • gpolder
    gpolder over 10 years ago in reply to DAB

    That was exactly the idea,

     

    Gerrit.