Pi IoT
  • Challenges & Projects
  • Design Challenges
  • Pi IoT
  • More
  • Cancel
Pi IoT
Blog [Pi IoT] Thuis #02: Collecting materials
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
  • Author Author: rhe123
  • Date Created: 26 May 2016 8:26 PM Date Created
  • Views 2103 views
  • Likes 5 likes
  • Comments 8 comments
  • hardware
  • piiot
  • thuis
Related
Recommended

[Pi IoT] Thuis #02: Collecting materials

rhe123
rhe123
26 May 2016

To make my proposal a reality I need quite some electronics in the house. Luckily we already have several Z-Wave devices and Raspberries in the house, and a sponsored Kit on the way. But what other hardware do we still need?

 

More Z-Wave devices

image

The entrance, living room, kitchen and office already have most lights controllable through Z-Wave. We do however plan to make this happen in the bedroom (and bathroom) as well to create a wake-up light. For this I’ll order the Fibaro Dimmer 2 or Qubino Dimmer modules, plus some dimmable LED bulbs and switches. Before ordering I’ll try to find out which combination is working best nowadays, because in the office I’m using the first generation Fibaro Dimmer and that one unfortunately buzzes while it’s dimmed. In a later blogpost I'll let you know which one I choose.

 

iBeacons

image

Next to PIRs I’ll be using iBeacons to detect where in the house we are. I’ve chosen the latest generation of Estimote beacons for this. I’ve used the first generation before and they are nice little beacons with a very powerful SDK. Using at least 6 beacons it should be possible to give a quite accurate approximation of your location in the house. I’ll be giving it a try when they arrive.

This generation is brand new, so I had to pre-order them.

MOVE

image

Another pre-order is the MOVE, which is currently available on Indiegogo. The MOVE is a bluetooth controlled motor to motorize existing blinds and shades. There is a micro USB connector as well which can be used to control it, so when it arrives I’ll experiment with both Bluetooth and USB control.

It will be used in the bedroom as part of the wake-up light. The estimated shipping date is currently in June.

 

HDMI capturing

For the ambilight in the home cinema I intend to use Hyperion. A HDMI splitter will be used so I can intercept the signal to the TV and feed into HDMI-to-RCA converter and a capturing device, which in turn will feed the images into a Raspberry Pi. The software interprets the image and controls the LEDs through an Arduino. Most materials are ordered from AliExpress, so it will probably arrive in about a month.

 

Patience

Now it’s time to be patience and wait for the arrival of all materials. In the meanwhile I’ll be working on some other parts, more about that in the next post!

  • Sign in to reply

Top Comments

  • fvan
    fvan over 10 years ago +3
    Some very recent tech you'll be using, that's cool! Unfortunately, it doesn't seem to be very affordable yet At 60EUR per dimmer and 33USD per beacon, the total cost of the project will increase rapidly…
  • mcb1
    mcb1 over 10 years ago +1
    Looks like a very interesting project. I do agree that the new tech is really nice, but the cost will get high fairly quickly. On the other side the commercial offerings aren't cheap or have as many features…
  • rhe123
    rhe123 over 10 years ago in reply to balearicdynamics +1
    Thanks again for your input balearicdynamics ! Just like you I bought a first set of iBeacons when they launched. In the beginning they were indeed limited in their purpose, but they did do their simple…
Parents
  • balearicdynamics
    balearicdynamics over 10 years ago

    Hi,

     

    I saw your post and I have a doubt, or at least a suggestion image Did you already tried to use the beacons? I bought their first version as they was announced and continued to follow the evolution but the updates (excluding the interlocutory email on how they was hard working during these last two years) was nothing more really meaningful. And I never found a serious SDK to put these products in condition to be really used in a real environment. I hope that now - I have abandoned their path by about six months - they have definitely solved the problems.

     

    BTW I agree with fvan that not only the commercial products are expensive, but also not always these grant something more than what can be done with few dollars and a sharp brain. The real thing that is blocking me adopting commercial products - excluding some very specific cases - is another: despite what will be the future destiny of your project anyway I suggest to think to it like something that will interest the market. This means that - why not? Hope and ambitions are free of charge image - in six months your prototype maybe ready to become a commercial product. So what happens if some of the commercial components become unavailable? Or, just in case, the company decide to change the product for any reason? This is the limit in cases like this; you (we) have no control at all on something that we buy closed in a box and IMHO it should not be a part of custom original project. Especially if it is a fundamental component.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rhe123
    rhe123 over 10 years ago in reply to balearicdynamics

    Thanks again for your input balearicdynamics! Just like you I bought a first set of iBeacons when they launched. In the beginning they were indeed limited in their purpose, but they did do their simple job well. Recently Estimote introduced the Indoor SDK which should have some interesting features. I didn't try this one yet, as you need at least two sets of beacons for a useful coverage. Another nice addition in their latest models is the GPIO slot, so it should be possible to hook them up to e.g. an Arduino.

     

    Considering commercial products, in my opinion it's about choices and priorities. Where in the system are the challenges in which you want to put effort and where you can do something innovative. In my case the challenge is to make everything work together nicely as a whole and less about e.g the individual bulbs. I do see the risk you mention regarding components becoming unavailable or changed. That's why in this case I chose for Z-Wave, which is a standard (be it not that open as I would like) backed by multiple manufacturers. And I'm not using one of the off-the-shelve controllers, but a pretty barebone Razberry which I control through their API. So for me this gives the freedom in the integration with other products (incl completely DIY), while having some reliable hardware connecting the lights. That those dimmers and plugs are compact and good-looking is an added bonus image

     

    Robin

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • rhe123
    rhe123 over 10 years ago in reply to balearicdynamics

    Thanks again for your input balearicdynamics! Just like you I bought a first set of iBeacons when they launched. In the beginning they were indeed limited in their purpose, but they did do their simple job well. Recently Estimote introduced the Indoor SDK which should have some interesting features. I didn't try this one yet, as you need at least two sets of beacons for a useful coverage. Another nice addition in their latest models is the GPIO slot, so it should be possible to hook them up to e.g. an Arduino.

     

    Considering commercial products, in my opinion it's about choices and priorities. Where in the system are the challenges in which you want to put effort and where you can do something innovative. In my case the challenge is to make everything work together nicely as a whole and less about e.g the individual bulbs. I do see the risk you mention regarding components becoming unavailable or changed. That's why in this case I chose for Z-Wave, which is a standard (be it not that open as I would like) backed by multiple manufacturers. And I'm not using one of the off-the-shelve controllers, but a pretty barebone Razberry which I control through their API. So for me this gives the freedom in the integration with other products (incl completely DIY), while having some reliable hardware connecting the lights. That those dimmers and plugs are compact and good-looking is an added bonus image

     

    Robin

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to rhe123

    Hi Robin,

    That's why in this case I chose for Z-Wave, which is a standard

    You focus the point. The choice of a widely diffused standard I think it is sufficient to justify the adoption of a commercial device. Anything occur, it can be replace as well. Better if the standard is open source.

     

    Enrico