Pi IoT
  • Challenges & Projects
  • Design Challenges
  • Pi IoT
  • More
  • Cancel
Pi IoT
Blog [Pi IoT] Thuis #02: Collecting materials
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
  • Author Author: rhe123
  • Date Created: 26 May 2016 8:26 PM Date Created
  • Views 2103 views
  • Likes 5 likes
  • Comments 8 comments
  • hardware
  • piiot
  • thuis
Related
Recommended

[Pi IoT] Thuis #02: Collecting materials

rhe123
rhe123
26 May 2016

To make my proposal a reality I need quite some electronics in the house. Luckily we already have several Z-Wave devices and Raspberries in the house, and a sponsored Kit on the way. But what other hardware do we still need?

 

More Z-Wave devices

image

The entrance, living room, kitchen and office already have most lights controllable through Z-Wave. We do however plan to make this happen in the bedroom (and bathroom) as well to create a wake-up light. For this I’ll order the Fibaro Dimmer 2 or Qubino Dimmer modules, plus some dimmable LED bulbs and switches. Before ordering I’ll try to find out which combination is working best nowadays, because in the office I’m using the first generation Fibaro Dimmer and that one unfortunately buzzes while it’s dimmed. In a later blogpost I'll let you know which one I choose.

 

iBeacons

image

Next to PIRs I’ll be using iBeacons to detect where in the house we are. I’ve chosen the latest generation of Estimote beacons for this. I’ve used the first generation before and they are nice little beacons with a very powerful SDK. Using at least 6 beacons it should be possible to give a quite accurate approximation of your location in the house. I’ll be giving it a try when they arrive.

This generation is brand new, so I had to pre-order them.

MOVE

image

Another pre-order is the MOVE, which is currently available on Indiegogo. The MOVE is a bluetooth controlled motor to motorize existing blinds and shades. There is a micro USB connector as well which can be used to control it, so when it arrives I’ll experiment with both Bluetooth and USB control.

It will be used in the bedroom as part of the wake-up light. The estimated shipping date is currently in June.

 

HDMI capturing

For the ambilight in the home cinema I intend to use Hyperion. A HDMI splitter will be used so I can intercept the signal to the TV and feed into HDMI-to-RCA converter and a capturing device, which in turn will feed the images into a Raspberry Pi. The software interprets the image and controls the LEDs through an Arduino. Most materials are ordered from AliExpress, so it will probably arrive in about a month.

 

Patience

Now it’s time to be patience and wait for the arrival of all materials. In the meanwhile I’ll be working on some other parts, more about that in the next post!

  • Sign in to reply

Top Comments

  • fvan
    fvan over 10 years ago +3
    Some very recent tech you'll be using, that's cool! Unfortunately, it doesn't seem to be very affordable yet At 60EUR per dimmer and 33USD per beacon, the total cost of the project will increase rapidly…
  • mcb1
    mcb1 over 10 years ago +1
    Looks like a very interesting project. I do agree that the new tech is really nice, but the cost will get high fairly quickly. On the other side the commercial offerings aren't cheap or have as many features…
  • rhe123
    rhe123 over 10 years ago in reply to balearicdynamics +1
    Thanks again for your input balearicdynamics ! Just like you I bought a first set of iBeacons when they launched. In the beginning they were indeed limited in their purpose, but they did do their simple…
  • rhe123
    rhe123 over 10 years ago in reply to fvan

    Z-Wave components are indeed quite costly, although it's doable when you grow the setup gradually. There are some cheaper brands available as well.

     

    Providing a cost breakdown at the end could be interesting indeed, I'll try to add it in one of my later blogs!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 10 years ago

    Looks like a very interesting project.

    I do agree that the new tech is really nice, but the cost will get high fairly quickly.

     

    On the other side the commercial offerings aren't cheap or have as many features.

     

    Many of the latest gadgets/offerings to the market are at a premium, but give it 5 years and they become much cheaper ... however has the associated tech moved on since then??

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fvan
    fvan over 10 years ago

    Some very recent tech you'll be using, that's cool! Unfortunately, it doesn't seem to be very affordable yet image

    At 60EUR per dimmer and 33USD per beacon, the total cost of the project will increase rapidly. I may consider implementing these solutions at home when they get cheaper though!

     

    Perhaps interesting to have a cost breakdown per project at the end of the challenge. Could be useful for anyone wishing to reproduce a project.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
<