Pi IoT
  • Challenges & Projects
  • Design Challenges
  • Pi IoT
  • More
  • Cancel
Pi IoT
Blog [PiIoT#06]: Ambient monitoring with Enocean sensors
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
  • Author Author: vish
  • Date Created: 17 Aug 2016 4:17 PM Date Created
  • Views 1388 views
  • Likes 3 likes
  • Comments 4 comments
  • python
  • vish_piiot
  • enocean-pi
  • piiot
  • enocean
  • enocean sensor kit
  • raspberry pi
  • piiot challenge
Related
Recommended

[PiIoT#06]: Ambient monitoring with Enocean sensors

vish
vish
17 Aug 2016

Enocean Sensors are wireless sensors working by energy harvesting from environment - no wires, no battery, no limits!!! In this post, I'll be using three sensors from the Enocean Sensor kit and EnoceanPi enable raspberry pi receive the data from sensors and forward it to a MQTT broker. This is later displayed in freeboard. I'll be using Python for receiving data from enocean sensors and sending it to MQTT broker.

 

Installing the sensors

image

Enocean Temperature sensor installed on my wall

image

Enocean Contact sensor installed at my door

 

Preparing your Pi

Not much has to be done in the Pi. We can directly connect the EnoceanPi gateway module to Pi3 (or any other Pi also). But it will block the entire GPIO will be blocked by the module. Since I would like to use some of those pins for other purposes, I thought of wiring only the required pins together and thus unblocking othe GPIO pins. As it turns out, EnoceanPi uses serial communication and hence require only four connection : 3V3, RXD, TXD, GND. So I decided to connect them using jumper wires.

 

Installing Paho MQTT Python Client

Next step is to install necessary MQTT library to Pi. I'll be using Paho MQTT Python library for this project. To install it, from your Pi's terminal

$ pip install paho-mqtt

This will install the necessary python libraries for communicating with an MQTT broker in your Pi.

 

Installing Enocean python library

For this challenge, I planned to reuse the Python library for enocean devices I developed during FMN challenge. I modified the library to detect individual sensors and added the basic three application style decoding for radio data. This will enable you to ge the raw data send by the enocean node on a nice object form which you can process later. To get the library clone my github repo using

$ git clone https://github.com/v-i-s-h/Enocean-Py.git

Inside the repo, under 'Enocean-Py/EnoceanPy/eopy.py', you can find a sample code for usage.

 

Let's code

Now we can code the main logic. This is what we are going to do. Whenever enoceanPi receives a telegram, we'll decode it and check whether it from temperature sensor or contact sensor. Then we'll send it on the topic user/vish/sensors/<sensor_id>.

The code is given below and is mostly self explanatory:

# Bridge.py


import sys, os, inspect


import time


from time import gmtime, strftime





# Add modules to path


libPath = os.path.abspath(os.path.join(os.path.dirname(__file__), "./../"))


if libPath not in sys.path:


  sys.path.insert(0, libPath)





from EnoceanPy import EO


from EnoceanPy import ESP





import paho.mqtt.client as mqtt


import paho.mqtt.publish as publish





basePath  = 'usr/vish/'


appPath  = 'sensors/'





## Define MQTT callbacks


def onConnect( client, userData, retCode ):


  client.publish( basePath+'devices/enocean', '{"name":"enocean gateway","desc":"ESP to MQTT bridge"}' );








def main():


   print "\t\t** Enocean bridge **"





  ttyPort = "/dev/ttyAMA0"


   print "\tEncoean gateway port : " + ttyPort + '\n'





   # CO_RD_IDBASE command


  cmd1 = [ 0x55, 0x00, 0x01, 0x00, 0x05, 0x70, 0x08, 0x38 ]





  hEOGateway = EO.connect( ttyPort )


   # better to wait a little for connection to establish


  time.sleep( 0.100 )





   ## display any packets already in buffer


   print "Buffered Packets : ",


  rawResp = EO.receiveData( hEOGateway )





   ## Send CO_RD_IDBASE


   print "RQST : ",


   for i in range( len( cmd1 ) ):


   print "%02X" %( cmd1[i] ),


   print ''


   #~ EO_receiveData( hEOGateway ) # Read any buffered data


  rawResp = EO.sendData( hEOGateway, cmd1 )


   print 'RESP(%3dB) : ' %len( rawResp ),


   for i in range( len( rawResp ) ):


   print "%02X" %(rawResp[i]),


   print ''


  pkt = ESP.decodePacket( rawResp )


   ESP.displayPacketInfo( pkt, 'CO_RD_IDBASE' )





   # Connect to broker


  client = mqtt.Client( client_id = "enocean_bridge",


   clean_session = True );


  client.on_connect = onConnect;


  client.connect( "192.168.1.54", 1883, 60 )


  client.loop_start();





   try:


   while( True ):


  rawResp = EO.receiveData( hEOGateway )


   if rawResp:


   print strftime("%Y-%m-%d %H:%M:%S",gmtime()),": ",


   print '[RXD] ',


   for i in range( len( rawResp ) ):


   print "%02X" %(rawResp[i]),


   print ''


  pkts = ESP.decodeRawResponse( rawResp )


   for pkt in pkts:


   # print " :> ",


   # for i in range(len(pkt['data_recv'])):


   # print "%02X" %(pkt['data_recv'][i]),


   # print ''


   # print "[PACKET]................................................................."


  telegram = ESP.decodeRadioData( pkt )


   if( telegram['dev'] != 'UNKN' ):  # Not an unknown telelgram


  mqttPacket = {}


  str_id = ""


   for i in telegram['id']:


  str_id = str_id + ("%02X" %i)


  mqttPacket['id'] = str_id;


   # Check which sensor send the telegram


   if telegram['dev'] == 'RCKR':


   # From rocker swicth


  action  = telegram['data'] & 0xE0


  bow  = telegram['data'] & 0x10


   if bow == 0x10:


   if action == 0x00:


  mqttPacket['action'] = 'AI'


   elif action == 0x01:


  mqttPacket['action'] = 'A0'


   elif action == 0x20:


  mqttPacket['action'] = 'BI'


   elif action == 0x30:


  mqttPacket['action'] = 'B0'


   else:


   print "%02X" %action


  mqttPacket['action'] = 'invalid'


   else:


  mqttPacket['action'] = 'released'


   elif telegram['dev'] == 'TEMP':  # From temperature sensor


   # 3rd byte in data is useful


  mqttPacket['temp'] = 20.0 + (60.0-20.0)/255*telegram['data'][2]


   elif telegram['dev'] == 'CNCT':


  mqttPacket['status'] = telegram['data']&0x01;





  str_mqtt = ', '.join("%s=%r" % (key,val) for (key,val) in mqttPacket.iteritems())


   print( str_mqtt )


  client.publish( basePath+appPath+str_id, str_mqtt );


   # print "........................................................................."


   except KeyboardInterrupt:


   print "\nExiting Enocean MQTT Brdige"


   EO.disconnect( hEOGateway )


  client.disconnect()

main()

 

This file is also available inside the repository, under PiIoT/bridge.py

Now you can run the bridge using

$ python bridge.py

This will create a new client from the Python app, connect to the broker specified and publishes a 'hello' message. Then for each of the telegrams received, it will forward it to the broker.

 

Later I'll be subscribing to the topics from the sensors using Freeboard dashboard to display the data.

That's all for this update

 

Happy Hacking,

vish

 

<< Prev | Index | Next >>

Attachments:
enocean2mqtt_bridge.py.txt.zip
  • Sign in to reply

Top Comments

  • DAB
    DAB over 10 years ago +2
    Nice update. It will be interesting to see what the maximum transfer rate will be when you get multiple sensors sending asynchronous data. DAB
  • vish
    vish over 10 years ago in reply to DAB +1
    Hi DAB, I dont think transfer rate could be a problem, as these sensors are sending a packet every 15 or 20 minutes, it's not going to chock the bandwidth really.
  • volly
    volly over 10 years ago

    DAB I really see no problem here.....all cool.....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 10 years ago in reply to vish

    Ah yes, the missing information.

     

    I agree, at that data rate, you are quite safe.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • vish
    vish over 10 years ago in reply to DAB

    Hi DAB,

    I dont think transfer rate could be a problem, as these sensors are sending a packet every 15 or 20 minutes, it's not going to chock the bandwidth really.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 10 years ago

    Nice update.

     

    It will be interesting to see what the maximum transfer rate will be when you get multiple sensors sending asynchronous data.

     

    DAB