PiCasso Design Challenge
  • Challenges & Projects
  • Design Challenges
  • PiCasso Design Challenge
  • More
  • Cancel
PiCasso Design Challenge
Blog PiCasso Design Challenge - Post 7 Part 2
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
  • Author Author: dwinhold
  • Date Created: 3 May 2019 12:48 AM Date Created
  • Views 1435 views
  • Likes 11 likes
  • Comments 7 comments
  • pov globe
  • picasso design challenge
  • dwinhold
Related
Recommended

PiCasso Design Challenge - Post 7 Part 2

dwinhold
dwinhold
3 May 2019

Welcome back for the 2nd part of my 7th blog. This part is the motor turning the globe, proving the sewing maching motor works. The video below shows it working.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Thank you

 

Dale W

  • Sign in to reply

Top Comments

  • balearicdynamics
    balearicdynamics over 7 years ago +5
    Dalem very great progress! I like the sound of this motor when runs; you saved the memory of the sewing machine sound. It remembers ancient moments when I was a kid and this sound was frequently present…
  • dwinhold
    dwinhold over 7 years ago in reply to balearicdynamics +5
    Hi Enrico I did run the globe for 15 minutes non-stop at high speed. The only issue I found was a slight vibration. The cause is the globe ring isn't 100% balanced yet (which I knew before). I even ran…
  • balearicdynamics
    balearicdynamics over 7 years ago in reply to dwinhold +5
    Hello Dale, I think that 15 minutes is already a good test. If nothing has broken, there are boog possibilities that it will rung for a very long period without problems. Enrico
Parents
  • dubbie
    dubbie over 7 years ago

    Dale,

     

    You have achieved a great solution, especially getting to be so balanced. For your project that is probably one of the major requirements, I think the wooden support structure shows how important a stable framework is for a project such as yours. It is very impressive. I also really like the fact that it still sounds like a sewing machine. It just shows that the sound of sewing comes from the motor and not from the rest of the mechanism - which is surprising.

     

    Having worked with rotating things before, having made a sizeable DC motor, I am always wary of things flying off, does your sustem have screens for you ro hide behind? I was made to use Perspex cages for my DC motor but I preferred to just stand to one side!

     

    It must be tempting to see how fast it might go, but then again, that might lead to destruction! How fast does it need to go to be effective with the LEDs? For most things to avoid flicker you need about 50 Hz which would be 3000 rpm.

     

    Dubbie

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dwinhold
    dwinhold over 7 years ago in reply to dubbie

    Hi Dubbie

    For safety I am making a lexan shroud. Safety first!! The motor has a speed of 4800rpm, I have the pully wheels at 2.5:1 so I'm getting 1920 rpm right now at full speed minus the globe weight and drag causing the motor to slow down.

    I have to say, this is the most fun project I have done. Learning lots and making something I wanted for a long time.

     

    Dale

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dwinhold
    dwinhold over 7 years ago in reply to dubbie

    Hi Dubbie

    For safety I am making a lexan shroud. Safety first!! The motor has a speed of 4800rpm, I have the pully wheels at 2.5:1 so I'm getting 1920 rpm right now at full speed minus the globe weight and drag causing the motor to slow down.

    I have to say, this is the most fun project I have done. Learning lots and making something I wanted for a long time.

     

    Dale