PiCasso Design Challenge
  • Challenges & Projects
  • Design Challenges
  • PiCasso Design Challenge
  • More
  • Cancel
PiCasso Design Challenge
Blog PiCasso Design Challenge - POV Globe Blog 12
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
  • Author Author: dwinhold
  • Date Created: 31 May 2019 2:13 AM Date Created
  • Views 2272 views
  • Likes 12 likes
  • Comments 12 comments
  • pov globe
  • picasso design challenge
  • led
  • dwinhold
Related
Recommended

PiCasso Design Challenge - POV Globe Blog 12

dwinhold
dwinhold
31 May 2019

Today I have an update of the POV globe. I spent some more time trying to program the lights to produce random colours. This was very successful as you will see with the photos below. I included the Python3 script.

 

import board
import random
import neopixel
import time
x = 0
pixels = neopixel.NeoPixel(board.D18, 72) #Setting the output pin to 18 and setting up 72 LEDs
while True:
 pixels[x] = ((random.randint(1, 255)), (random.randint(1, 255)), (random.randint(1, 255)))  #Randomise colour
 time.sleep(.01) #Delay 100th of a second
 x = x + 1
 if x > 71: #Since there are 72 LEDs reset to the start
  x = 0

 

The script isn't very long but works great!!

 

I have been working on programming the planet but that will be an all summer job. I created a graph to show how much work it will be to program. I divided the world into a grid so I can address the LED's correctly to display the world. And yes, I did draw this out myself...

 

image

 

Below are photos of the new script running on the globe. Hope you enjoy!!

 

image

 

image

 

image

 

As you can see, in each photo the LEDs are a different colour. I love sitting and watching the globe, it is hypnotizing.

 

Thank you for reading

 

Dale Winhold

  • Sign in to reply

Top Comments

  • dougw
    dougw over 7 years ago +6
    This is a fabulous project with outstanding execution. Photographing flashing LEDs will always be highly problematic. If you can get a static pattern and take a time exposure through dark sunglasses, the…
  • dixonselvan
    dixonselvan over 7 years ago +4
    dwinhold wow really the LEDs are hypnotizing! Hope there should be an easy way to implement the world map in the globe. I assume the below can be a way we can implement it, 1. Take an image of the world…
  • jc2048
    jc2048 over 7 years ago +4
    Very nicely done - I wish I had your construction skills. It's going to look quite superb when you have the globe spinning in there. How does the Pi know where it is when it's displaying? Do you have a…
Parents
  • dixonselvan
    dixonselvan over 7 years ago

    dwinhold wow really the LEDs are hypnotizing!

     

    Hope there should be an easy way to implement the world map in the globe. I assume the below can be a way we can implement it,

     

    1. Take an image of the world map

    2. Convert into pixel values

    (https://stackoverflow.com/questions/43719451/python-convert-image-to-a-string-of-pixel-values  - this could help)

    3. Map pixel values to RGB LED matrix

    4. This could be tricky, we will now have a format which can be displayed in flat displays something like matrix displays/ monitor etc. We have to convert it to a single strip column wise and move it column by column. Like C1 then C2 till Cn the viewer should have a glimpse of C1 to Cn in the same time. (Let me know if this is confusing)

    5. You will now have a static image of the world map ... then you can try animations!

     

    This is a very high level approach and I am not sure if this will work since I haven't tried it so far ... let me keep you posted if I find some more help!

     

    Thanks,

    Dixon Selvan

     

    Edit:

    I think adding black foam or any non-reflecting substance in the box holding the globe would make it look like only the globe is present. However the current version is cool as well!

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dixonselvan
    dixonselvan over 7 years ago

    dwinhold wow really the LEDs are hypnotizing!

     

    Hope there should be an easy way to implement the world map in the globe. I assume the below can be a way we can implement it,

     

    1. Take an image of the world map

    2. Convert into pixel values

    (https://stackoverflow.com/questions/43719451/python-convert-image-to-a-string-of-pixel-values  - this could help)

    3. Map pixel values to RGB LED matrix

    4. This could be tricky, we will now have a format which can be displayed in flat displays something like matrix displays/ monitor etc. We have to convert it to a single strip column wise and move it column by column. Like C1 then C2 till Cn the viewer should have a glimpse of C1 to Cn in the same time. (Let me know if this is confusing)

    5. You will now have a static image of the world map ... then you can try animations!

     

    This is a very high level approach and I am not sure if this will work since I haven't tried it so far ... let me keep you posted if I find some more help!

     

    Thanks,

    Dixon Selvan

     

    Edit:

    I think adding black foam or any non-reflecting substance in the box holding the globe would make it look like only the globe is present. However the current version is cool as well!

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • dwinhold
    dwinhold over 7 years ago in reply to dixonselvan

    Dixon, thank you so much for the information. I will see what I can come up with. I need all the help possible.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dixonselvan
    dixonselvan over 7 years ago in reply to dwinhold

    Happy to help image