PiCasso Design Challenge
  • Challenges & Projects
  • Design Challenges
  • PiCasso Design Challenge
  • More
  • Cancel
PiCasso Design Challenge
Blog PiCasso Design Challenge - POV Globe Blog 3
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
  • Author Author: dwinhold
  • Date Created: 4 Apr 2019 12:49 AM Date Created
  • Views 1263 views
  • Likes 10 likes
  • Comments 9 comments
  • pov
  • pov globe
  • picasso design challenge
  • led
  • dwinhold
  • globe
Related
Recommended

PiCasso Design Challenge - POV Globe Blog 3

dwinhold
dwinhold
4 Apr 2019

Hi everyone,

 

This weeks update is a bit more then I figured. I got quite a bit completed on the building of the globe. As you will see I created the base for the globe, top part to support the north end of the globe and have the LED's attached. I am trying to see if I can make it more 3D by giving it depth with a second row of LED's on the inside of the globe. This way I can produce 2 pictures at 2 different depths at the same time. As always, anyone want any of the .dxf files for this project please ask, I will send them out!!

 

Below are pictures of the globe so far:

 

Outside row of LED's

image

Inside Row of LED's

image

Support post in the bearings

image

 

I had to firgue out how to power the RPi and the LED's. Since the globe is spinning, I can't just run the power cord to the hardware for obvious reasons. I plan on using the bearings as the power connection. One for the positive and one for the negative. I will attach one half of the wire to the outside of the bearing and the other half to the inside. Hope it works!!

 

Below is a very short video of the globe turning (By hand) no motor is hooked up yet.

 

This will be my next blog, hooking up the motor.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Thank you for reading,

 

Dale Winhold

 

  • Sign in to reply

Top Comments

  • balearicdynamics
    balearicdynamics over 7 years ago +6
    Good progress, Dale. I appreciate the cleanliness of the design, very well done. Enrico
  • dubbie
    dubbie over 7 years ago +6
    Dale, A very smooth turning action. The bearings must be working well. Have you given any thought to the wind or draught that might be created? For a flicker free image you might need to rotate at 50 revolutions…
  • maegeph
    maegeph over 7 years ago +6
    I've seen someone using an audio jack to transfer power, very clever idea https://hackaday.com/2009/10/15/72-led-persistence-of-vision-globe/
Parents
  • dubbie
    dubbie over 7 years ago

    Dale,

     

    A very smooth turning action. The bearings must be working well. Have you given any thought to the wind or draught that might be created? For a flicker free image you might need to rotate at 50 revolutions per second or maybe only 25 revs per second if using both sides of the globe. which is going to move a lot of air around.

     

    Dubbie

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dwinhold
    dwinhold over 7 years ago in reply to dubbie

    Hi Dubbie

     

    Speed is something I will have to be playing with. G-force, wind and draught is a bit of a concern and will have to be dealt with if it becomes a problem.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dwinhold
    dwinhold over 7 years ago in reply to dubbie

    Hi Dubbie

     

    Speed is something I will have to be playing with. G-force, wind and draught is a bit of a concern and will have to be dealt with if it becomes a problem.

    • Cancel
    • Vote Up +6 Vote Down