PiCasso Design Challenge
  • Challenges & Projects
  • Design Challenges
  • PiCasso Design Challenge
  • More
  • Cancel
PiCasso Design Challenge
Blog Something is still missing
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
  • Author Author: apn201
  • Date Created: 7 Mar 2019 8:36 PM Date Created
  • Views 1355 views
  • Likes 9 likes
  • Comments 8 comments
  • led matrix
  • picasso design challenge
  • raspberry pi 3b+
  • 8x8 led matrix
Related
Recommended

Something is still missing

apn201
apn201
7 Mar 2019

A While ago I got a new shipment. It's a 8X8 LED matrix kit for Raspberry Pi. The idea is that I'll assembly the kit and use it to practice programming on the device - and then eventually I'll just replace the LEDs with resistors or something.. at least that's the theory.

I'm still missing something and that is the motivation to start. I know once I start, things will move quickly as I cannot leave any problem unsolved, but also, as I know that this project will consume all my free time for some weeks. I'm afraid to start.


image

  • Sign in to reply

Top Comments

  • dougw
    dougw over 7 years ago +5
    That is a common problem and of course there are no easy solutions. It sometimes works to break it down into very small tasks so it is really quick to complete one task, but until you actually do one the…
  • jc2048
    jc2048 over 7 years ago +4
    Have you considered resistance wire rather than resistors? If you wound it in a spiral and glued it to the back of the thermochromic material it might allow for larger, more even pixels than with actual…
  • apn201
    apn201 over 7 years ago in reply to jc2048 +4
    That's a good idea. Frankly I have not yet been thinking so far. My plan was first to figure out how to control a matrix display with the LED-unit and maybe trying to connect it to the camera etc. Once…
Parents
  • dougw
    dougw over 7 years ago

    That is a common problem and of course there are no easy solutions.

    It sometimes works to break it down into very small tasks so it is really quick to complete one task, but until you actually do one the fear is still a deterrent.

    And even after doing something, the fear doesn't necessarily go away. image

    At least this community will appreciate it when you do overcome the inertia....image

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dougw
    dougw over 7 years ago

    That is a common problem and of course there are no easy solutions.

    It sometimes works to break it down into very small tasks so it is really quick to complete one task, but until you actually do one the fear is still a deterrent.

    And even after doing something, the fear doesn't necessarily go away. image

    At least this community will appreciate it when you do overcome the inertia....image

    • Cancel
    • Vote Up +5 Vote Down