PiCasso Design Challenge
  • Challenges & Projects
  • Design Challenges
  • PiCasso Design Challenge
  • More
  • Cancel
PiCasso Design Challenge
Blog When is a project finished?
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
  • Author Author: therepairatrooper
  • Date Created: 8 Jul 2019 6:06 AM Date Created
  • Views 3577 views
  • Likes 9 likes
  • Comments 12 comments
Related
Recommended

When is a project finished?

therepairatrooper
therepairatrooper
8 Jul 2019

I am asking myself this question because at this point, I have a working prototype but in that process I have also come to some conclusions.

 

In terms of finished, I have completed the window frame, connected my security camera and demonstrated the project working. Based on the conclusions below, this particular project is completed but opens doors for a more advanced project.

 

In reaching this end point, the following conclusions have become apparent:

 

1. That in order to appear natural, a much higher resolution source is required, which would also require a 4K monitor and a PI able to drive it.

2. A 32" TV is too small to be a convincing window, unless it was in perhaps a small prison cell

3. This concept has merit beyond creating a fake window. Windows with embedded lcd films in them could be used to provide someone on the 24th floor of a tower with a view of a park, rather than another building.

  • Sign in to reply

Top Comments

  • dougw
    dougw over 7 years ago +8
    4 thresholds = done : nothing significant left to learn potential satisfaction from further progress is insignificant the result of progress has no use nobody else is interested 4 thresholds = pause :…
  • dubbie
    dubbie over 7 years ago +7
    When is a project finished? A very philosophical question. It's a bit like asking 'How long is a piece of string?' Of all the projects I have been involved with I do not think any of them could be classed…
  • Jan Cumps
    Jan Cumps over 7 years ago +7
    (not talking for my professional life. Paycheck blurs the border): my projects are finished; When I can't be bothered searching for them when I have an improvement idea. When I don't come up with improvements…
Parents
  • Jan Cumps
    Jan Cumps over 7 years ago

    (not talking for my professional life. Paycheck blurs the border):

    my projects are finished;

    • When I can't be bothered searching for them when I have an improvement idea.
    • When I don't come up with improvements.
    • When turning on the soldering iron feels like homework
    • When broken and not in a mood to fix
    • When not used by myself as a product
    • When someone asks a question and I say that the forum is the best place to ask such questions ...
    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Jan Cumps
    Jan Cumps over 7 years ago

    (not talking for my professional life. Paycheck blurs the border):

    my projects are finished;

    • When I can't be bothered searching for them when I have an improvement idea.
    • When I don't come up with improvements.
    • When turning on the soldering iron feels like homework
    • When broken and not in a mood to fix
    • When not used by myself as a product
    • When someone asks a question and I say that the forum is the best place to ask such questions ...
    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Jan Cumps
    Jan Cumps over 7 years ago in reply to Jan Cumps

    (

    You can see this on the electronic load. My goal was to provide a programmable front end to an existing analog load and to learn delivering a professional API for automation.

    And show off skills to build good PCB designs.

    Whenever there was something related to the analog part , the DACs or ADCs, I never made a design decision. I asked Robert Peter Oakes or jc2048. Every time.

    Whenever there was something related to automating it, I made my own decisions (sometimes - not always: Peter talked me out of implementing the feedback loop in software -  neglecting the two afford-mentioned individuals image ).

    The automated part is still the only corner I design actively.

    )

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 7 years ago in reply to Jan Cumps

    Jan Cumps, you dont give yourself enough credit. You designed several great iterations of the PCBs, all the software related to implementing SCPI interface etc (All I did was the C# test app). I may have provided the initial designs that the analog DAC/ADC/Feedback stuff but you have lead the show for the last few years.

     

    I would say your name deserves to be on the PCB etc, not mine, and you deserve most of the credit.

     

    Keep up the great work.

    • Cancel
    • Vote Up +4 Vote Down