PiCasso Design Challenge
  • Challenges & Projects
  • Design Challenges
  • PiCasso Design Challenge
  • More
  • Cancel
PiCasso Design Challenge
Blog When is a project finished?
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
  • Author Author: therepairatrooper
  • Date Created: 8 Jul 2019 6:06 AM Date Created
  • Views 3585 views
  • Likes 9 likes
  • Comments 12 comments
Related
Recommended

When is a project finished?

therepairatrooper
therepairatrooper
8 Jul 2019

I am asking myself this question because at this point, I have a working prototype but in that process I have also come to some conclusions.

 

In terms of finished, I have completed the window frame, connected my security camera and demonstrated the project working. Based on the conclusions below, this particular project is completed but opens doors for a more advanced project.

 

In reaching this end point, the following conclusions have become apparent:

 

1. That in order to appear natural, a much higher resolution source is required, which would also require a 4K monitor and a PI able to drive it.

2. A 32" TV is too small to be a convincing window, unless it was in perhaps a small prison cell

3. This concept has merit beyond creating a fake window. Windows with embedded lcd films in them could be used to provide someone on the 24th floor of a tower with a view of a park, rather than another building.

  • Sign in to reply

Top Comments

  • dougw
    dougw over 7 years ago +8
    4 thresholds = done : nothing significant left to learn potential satisfaction from further progress is insignificant the result of progress has no use nobody else is interested 4 thresholds = pause :…
  • dubbie
    dubbie over 7 years ago +7
    When is a project finished? A very philosophical question. It's a bit like asking 'How long is a piece of string?' Of all the projects I have been involved with I do not think any of them could be classed…
  • Jan Cumps
    Jan Cumps over 7 years ago +7
    (not talking for my professional life. Paycheck blurs the border): my projects are finished; When I can't be bothered searching for them when I have an improvement idea. When I don't come up with improvements…
  • shabaz
    shabaz over 7 years ago in reply to dubbie

    Hehe in the south of England, that company was working on a videophone (GEC-Plessey) which I remember seeing on a school work-experience type trip. It looked really fancy for the time (passive-matrix TFT screen about 5 inches in size). But the technology wasn't quite there yet.. it needed a fat cable to the encoding hardware (maybe H.263) and interface (to ISDN BRI probably) which were in a massive box the size of a desktop PC, hidden under the desk : )

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 7 years ago

    When is a project finished? A very philosophical question. It's a bit like asking 'How long is a piece of string?' Of all the projects I have been involved with I do not think any of them could be classed as actually finished. The nearest would be the telephone tester  I designed and built when first employed as a Design Engineer with GEC Telecomms Ltd in the north of England. It was in a box and everything ready to go onto the production floor and then I left the company. But, one of the tests was an environmental temperature test but as I had no idea how to implement that so I just kind of skipped over it (Schhh, don't tell anyone!).Test 20 I think it was, which every telephone would always pass. To this day I still regret not getting help to implement that test. Good job mobile phones were invented and the company went bust - but I don't think that was all my fault.

     

    Dubbie

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • More
    • Cancel
<