Pi Chef Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Pi Chef Design Challenge
  • More
  • Cancel
Pi Chef Design Challenge
Blog Cracked pepper sir? (Delays and Detours...) Pi Chef Challenge Blog post #7
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
  • Author Author: crackedpepper
  • Date Created: 5 Mar 2018 11:00 AM Date Created
  • Views 797 views
  • Likes 5 likes
  • Comments 1 comment
Related
Recommended

Cracked pepper sir? (Delays and Detours...) Pi Chef Challenge Blog post #7

crackedpepper
crackedpepper
5 Mar 2018

So unfortunately i didn't make a post last week. While i was trying to get the parts printed i started having some problems with the 3D printer I was using. During the print layers would start offsetting as the print got further. The following image is the best print i could produce after this issue occurred image

image

I tried quite a few things but couldn't seem to overcome this problem. I eventually tried to update the firmware, this lead to more problems as the new firmware wouldn't install. At this point i decided i would be better off trying to make the arm the old fashioned way. This weeks post is the progress i have made so far.

 

I started off with a planning session on how to build the arm. All of my drawings are scribbles on paper so I am omitting them from this post (hopefully next week i will have a chance to produce some better diagrams to upload for the rest of the arm).

 

An overview of the base is as follows:

image

The M8 bolts only make contact with the inside of the bearings and I planned to drill the plate with a 12mm hole so that it will only make contact with the outside of the bearings. The motor would be mounted to the plate marked as the arm mount. For the base of the arm i decided to use a 125mm PVC pipe cap as that would be strong and it saved me from making something similar from scratch. To add some weight to it I attached a steel plate on the underside of the cap, this can be seen in the following image.

image

As I mentioned previously I had some bearings which i bought for the 3D printed arm which I originally planned to make. It was fairly easy to mount them as described in the diagram above, the following images show my questionable work making a bearing sandwich:

image

image

The bolts coming out of the top of the plate are for mounting the servo motor which will rotate the arm. The full setup can be seen with the mounted motor in this youtube video.. I was simply running the motor using an interactive python session image

 

Hopefully next week i can make significant progress in producing the rest of the arm.

  • Sign in to reply

Top Comments

  • genebren
    genebren over 8 years ago +2
    Good update. Sometimes things get in the way of progress, but trying to find solutions is also another type of progress. Keep up the good work! Gene
Parents
  • genebren
    genebren over 8 years ago

    Good update.  Sometimes things get in the way of progress, but trying to find solutions is also another type of progress.  Keep up the good work!

    Gene

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • genebren
    genebren over 8 years ago

    Good update.  Sometimes things get in the way of progress, but trying to find solutions is also another type of progress.  Keep up the good work!

    Gene