• Products and Partners
    Products and Partners
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
Pi Chef Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Pi Chef Design Challenge
  • More
  • Cancel
Pi Chef Design Challenge
Blog PiChef - SafeDegree Blog #2
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
  • Author Author: mark.gitsham
  • Date Created: 14 Feb 2018 2:14 PM Date Created
  • Views 989 views
  • Likes 7 likes
  • Comments 6 comments
Related
Recommended

PiChef - SafeDegree Blog #2

mark.gitsham
mark.gitsham
14 Feb 2018

Firstly, I would like to apologise in the tardiness of having my second blog uploaded. As Murphy’s Law always does I experienced a catastrophic kitchen accident that resulted in wine being spilled on my laptop… Maybe I should be concentrating on build a “Self Balancing Wine Glass”??

 

Expect a more thorough explanation and more photos when I build the second sensor unit and either edit this blog with the additional information, or another blog in-line.

 

 

Goals for this Blog

So, welcome back to my little project. Thanks to Newark and Element 14 - my kit finally arrived, along with the few extra bits and pieces I needed - such as a case, RaspberryPi Zero W, temp sensors and components to go…

 

Also thanks to the comments and support to those fellow engineers that have already commented on my first post. A couple of you asked about the process of automation and and regulations. After a quick chat with the in-laws, the only requirement they have is to ensure the temperature is recorded prior to first food being removed for use each day, temperature recording at end of day and a monthly calibration check to ensure the thermometer is within specification. For this, they have been using another digital thermometer and comparing to the already fixed cool room thermometer and fridge thermometers. Another suggestion was to install a door sensor - this will be something I will look at as an extra option.

 

Finally, there were suggestions to utilise a NFC reader to log who conducted the check and also for as an access logging. At this stage I probably won’t be looking at this as an option - time pending really, as the staffing is not that large and it is the responsibility of the shift manager to ensure alarms are acknowledged and responded to.

 

For this week, I plan to have the majority of the electronics completed, with testing happening as I go. This will include the build of the DS18B20 sensor leads, installation of the units into their appropriate housings and will also include remote sensor builds.

 

Master Unit

So there will be just a slight change in design from original concept Originally I was going to have the master unit also operate as a sensor But due to the lateness in the arrival of my kit it was not going to allow enough time to get a PCB manufacture to allow the splitting of the SPI port to allow the use of the  4DPI-24-HAT4DPI-24-HAT and and DS18B20

 

Now I will using the main unit only as the primary display logging reporting etc So for this I will only be using the Raspberry Pi 3 and the  4DPI-24-HAT4DPI-24-HAT a case and that will be all

 

A late addition - a small speaker to function as a audible buzzer to grab the attention of the operator.


image

 

Sensor Units

The sensor unit will be based on the Raspberry Pi Zero W, and include a DS18B20 temperature sensor, and after a quick design thought (thanks to others) a magnetic reed switch as a door sensor.

 

One of the advantages of using the DS18B20 sensor is they are utilise the “One-Wire” protocol and include a unique identification code. This will allow more than one sensor per Raspberry Pi Zero W to for use in Fridge / Freezer type scenarios or colocated cooling appliances (even ambient monitoring)

 

With that in mind, the only other comment required for the temperature sensor is a 4.7k resistor to go between the Data and Power pin. Only one resistor is required for the whole “One-Wire” network, so then the next sensor is simply connected in parallel.

image

To allow the operator to know the operation of the sensor, A tri colour LED will be installed showing basic operational states. A 330ohm resistor is connected to both anode pins of the LED.

image

As suggested by others, I will include the provision for a Magnetic Reed switch. This only requires a 10k resistor to tie the normally open switch pin to keep the pin from “floating” and tie it high.

image

As I mentioned earlier, I will update or re-blog a more thorough build for the sensor as there is some fun details to be included. But as an interim here is a photo of the completed unit - product labels are hopefully on there way.

image

image

What Is Next…

My next blog, will hopefully be out in the next couple of days where I will be starting the software install and configuration of the Master Unit.

  • Sign in to reply

Top Comments

  • genebren
    genebren over 8 years ago +1
    Good progress on your project. Too bad about the laptop and the wine. Did you laptop survive? Or is it still in rehab? Keep up the good work, looking forward to updates on your project. Gene
  • mark.gitsham
    mark.gitsham over 8 years ago in reply to genebren +1
    Thanks Gene, Unfortunately the laptop didn't survive, and haven't had a chance to connect the HDD to a SATA adaptor to see if it survived... I'm doubtful though as it had a good drink
  • DAB
    DAB over 8 years ago +1
    Nice update. DAB
Parents
  • genebren
    genebren over 8 years ago

    Good progress on your project.  Too bad about the laptop and the wine.  Did you laptop survive?  Or is it still in rehab?  Keep up the good work, looking forward to updates on your project.

    Gene

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • genebren
    genebren over 8 years ago

    Good progress on your project.  Too bad about the laptop and the wine.  Did you laptop survive?  Or is it still in rehab?  Keep up the good work, looking forward to updates on your project.

    Gene

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • mark.gitsham
    mark.gitsham over 8 years ago in reply to genebren

    Thanks Gene,

     

    Unfortunately the laptop didn't survive, and haven't had a chance to connect the HDD to a SATA adaptor to see if it survived... I'm doubtful though as it had a good drink image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 8 years ago in reply to mark.gitsham

    Mark,

     

    Best of luck with reviving the HHD.  Hopefully any important data will be recovered.

     

    Gene