Pi Chef Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Pi Chef Design Challenge
  • More
  • Cancel
Pi Chef Design Challenge
Blog Stove Assistant - Bernhard - Pi Chef #1 - Introduction
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
  • Author Author: bernhardmayer
  • Date Created: 25 Jan 2018 6:51 AM Date Created
  • Views 1245 views
  • Likes 8 likes
  • Comments 7 comments
  • pi_chef
  • baking
  • pancake
  • temperaturedetection
  • grid-eye®
  • cooking
  • raspberry_pi_design_challenge
Related
Recommended

Stove Assistant - Bernhard - Pi Chef #1 - Introduction

bernhardmayer
bernhardmayer
25 Jan 2018

Stove Assistant - Introduction

 

Cooking is sometimes difficult. At least for me. Not so much for my wife or my mother. Especially for some meals like pancakes. When I cook them are always partly stiff but also doughy. I think this is because I work at the wrong temperature or let them too long in the pan.

 

This is where my stove assistant comes in. He will check the actual temperatures and have an eye on the clock and help me to cook pancakes as good as my wife.

 

The setup

Therefore a pi camera together with a temperature sensor is placed atop of the cooktop of the stove I will use the Panasonic Grid-Eye Infrared Array Sensor  AMG8834AMG8834 http://uk.farnell.com/panasonic-electronic-components/amg8834/temperature-sensor-ir-3deg-c-module/dp/2576420) as temperature sensor.

 

Here is a mock-up of the stove assistant installation: (Sorry, I am not so good at photoshop. You get a better picture at the end of the project)

image

 

The camera and the temperature sensor will be aligned so that there is temperature information for every section of the image. The camera will be used to identify the used part of the cooktop (where the pan is placed). I want to implement this with OpenCV and maybe the use of deep neural networks if applicable.

The HMI can be done by a display with touch next to the Raspberry Pi. But the Raspberry Pi has to be mounted atop of the cooktop so this could be difficult to reach and read. So i will check if it is more practicable to do a remote HMI on a smartphone via Wifi.

 

Description of the cooking process:

  1. The user starts the system
  2. The user chooses to make pancakes on the HMI of the Raspberry Pi
  3. The user places the pan on the cooktop and heats it up.
  4. The Raspberry Pi automatically checks where the pan is placed and checks its temperature
  5. The Raspberry Pi gives notice to the user when the right startup temperature is reached.
  6. The user places the paste in the pan.
  7. The Raspberry Pi checks the temperature of the pancake and gives notice to the user when it is the right time to turn the pancake (by monitoring its temperature and the baking time)
  8. The Raspberry Pi checks the temperature of the now turned pancake and gives notice to the user when it is finally baked (by monitoring its temperature and the baking time)
  9. The user can go to step 5 and bake a new pancake or finish the cooking.

 

The proceeding of the steps will be recognized by the Raspberry Pi by image detection.

During the whole process the temperature is monitored and advice is given to the user by the system to turn the heat of the cooktop up or down. Unfortunately the Raspberry Pi can't directly control the heat of a cooktop without modification of the cooktop. So the stove assistant is limited to tell the user to change the heat.

As a side effect the temperature profile of the whole cooking process is monitored and can be compared with an optimal profile to give the user hints how to improve his cooking.

 

Project plan

I plan to go through the project according to the following plan. There will be one or two blog posts for each step. If new challenges arrise during the process of the project this plan can be adopted.

  • Unboxing, bring up Rapsberry Pi and camera with OpenCV
  • connect infrared sensor to Raspberry Pi and read out temperature information
  • check alignment of temperature sensor and camera
  • implement a graphic algorithm with OpenCV to identify the active part of the cooktop (where the pan is placed)
  • implementation of the HMI
  • do  some test cookings and record the temperature profile
  • write the main program to guide the user through the cooking
  • do more testing and tasting

 

additional steps (if accidentally time is left)

  • get the user feedback on the taste of the meal and optimize the process automatically
  • adopt the project to other meals.

 

Risks

As with every project there are some risks that could delay the project or prevent the realisation. If you identify most of them in advance you have a good chance to avoid them.

  • pollution of the sensors by smoke and steam of the cooking process could impact the measurements.
  • reflections prevent correct temperature measurements
  • low WAF

 

Future development

When the project works out well it could be adopted to other uses or expand its functionality

  • Identify more meals where this sensor could help
  • connect with an online database to exchange recipes and temperature profiles
  • prepare several meals simultaneously
  • find a cooktop where the heat can be influenced directly so that automatic cooking is possible
  • connect to home automation
  • Sign in to reply

Top Comments

  • genebren
    genebren over 8 years ago +4
    Very interesting project! Will there be a pancake party at the conclusion of the project?
  • three-phase
    three-phase over 8 years ago +3
    Good introduction to your project. I like the way you have worked your way logically through your proposal. Good luck with the forthcoming design and build. Kind regards
  • beacon_dave
    beacon_dave over 8 years ago +3
    could you perhaps use a 45degree mirror to take the camera out of the steam zone ? if it was heated then it may demist it as well.
Parents
  • beacon_dave
    beacon_dave over 8 years ago

    could you perhaps use a 45degree mirror to take the camera out of the steam zone ?

    if it was heated then it may demist it as well.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • beacon_dave
    beacon_dave over 8 years ago

    could you perhaps use a 45degree mirror to take the camera out of the steam zone ?

    if it was heated then it may demist it as well.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • bernhardmayer
    bernhardmayer over 8 years ago in reply to beacon_dave

    Hi Dave,

    thanks for your suggestion.

    I plan to do some test at the end of next week and see how bad it gets.

    When I use a mirror I still have the problem that the mirror gets dirty. So you still have to clean the mirror. Maybe I get the same result if I simply place a cover window in front of the cameras. It is always easier to clean the cover window than to clean the camera itself.

    I will tast this.

    Bernhard

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 8 years ago in reply to bernhardmayer

    I was thinking that the mirror would be less impacted by the steam penetration and easier to wipe clean than an overhead camera module. However a good sealed cover for the camera would also work, although unless it is made of glass, then perhaps it may be difficult to scrub clean without scratching it in the process.