Pi Chef Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Pi Chef Design Challenge
  • More
  • Cancel
Pi Chef Design Challenge
Blog Stove Assistant - Bernhard - Pi Chef #5 - First Test at the Cooktop
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
  • Author Author: bernhardmayer
  • Date Created: 19 Mar 2018 11:35 AM Date Created
  • Views 743 views
  • Likes 7 likes
  • Comments 1 comment
  • weisswurst
  • grid-eye®
  • designchallenge
  • raspberry3
  • raspberry_pi_design_challenge
  • pichef
Related
Recommended

Stove Assistant - Bernhard - Pi Chef #5 - First Test at the Cooktop

bernhardmayer
bernhardmayer
19 Mar 2018

Today I made my first test at the cooktop.

 

Test measurement

 

I somehow mounted the camera array and the Raspberry Pi above the cooktop (you don't want to see any pictures, believe me) and started the measurement. Today my family planed to have weißwurst (https://en.wikipedia.org/wiki/Weisswurst) for brunch and I used the change. These sausages are already cooked, so you only have to heat them up to have a warm meal. On the other hand you have to avoid to boil them because then the sausages will explode. So heating them up is a little bit complicated if you want your sausages hot. Perfect for the stove assistant!

 

Here is the video. It is 15 times faster than in reality.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

The stove assistant also saved the temperature profile (all values in degrees celsius):

image

For the first test I didn't make any complex image recognition and temperature detection. I simply took the highest measured of the grid-eye sensor and assumed that this is the temperature in my pot. As long as there is only one pot at the cooktop this should be OK.

 

Findings

There are some interesting findings:

  • The spikes in the temperature profile always accured when I stirred with a spoon. So I assume the temperature at the surface (which the grid-eye sensor can measure) is about 10 degrees celsius colder than the actual temperature in the pot.
  • It seemed that the water was nearly boiling although the sensor measured only 60 oder (when stirred) 70 degrees celsius.

 

So I definitely have to make more tests and measurements.

Brunch

 

Nevertheless we managed to heat up the sausages corectly:

image

What's next:

more measurements ...

And a new camera mount above the cooktop and start with the HMI.

  • Sign in to reply
Parents
  • genebren
    genebren over 8 years ago

    Bernhard,

     

    I noticed the increase temperatures during stirring in the videos.  I don't know for sure, but by stirring, you might be breaking the thermal contact of the food from the pan.  With decreased contact, the 'heatsink' is removed and the temperature rises.  Interesting observation.

    Gene

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • genebren
    genebren over 8 years ago

    Bernhard,

     

    I noticed the increase temperatures during stirring in the videos.  I don't know for sure, but by stirring, you might be breaking the thermal contact of the food from the pan.  With decreased contact, the 'heatsink' is removed and the temperature rises.  Interesting observation.

    Gene