Pi Chef Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Pi Chef Design Challenge
  • More
  • Cancel
Pi Chef Design Challenge
Blog Stove Assistant - Bernhard - Pi Chef #6.5 - Tests with bigger pot
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
  • Author Author: bernhardmayer
  • Date Created: 26 Mar 2018 10:16 PM Date Created
  • Views 751 views
  • Likes 7 likes
  • Comments 2 comments
  • testing
  • video
  • grideye
  • grid-eye®
  • designchallenge
  • raspberry3
  • raspberry_pi_design_challenge
  • pichef
Related
Recommended

Stove Assistant - Bernhard - Pi Chef #6.5 - Tests with bigger pot

bernhardmayer
bernhardmayer
26 Mar 2018

Today I made another test at the cooktop. This time I boiled water in a bigger pot to see if the grid eye sensor gets the temperature right when there is a bigger area below the sensor at a higher temperature.

 

Here is the video:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

It turned out that it is a little bit better but still not sufficient. The measured temperature is now at about 70 degrees celsius when the water is boiling. But there are now also samples in between where the temperature goes up to nearly 100 degrees celsius.

 

My next thought was that maybe the grid-eye sensor is not measuring the temperature of the water surface in the pot but instead the temperature of the steam between pot and sensor. I tried to eliminate this by blowing the steam away with a fan but it didn't change anything on the measurements.

 

To get this measurement right I made a new setup. Instead of boiling water I heated cooking oil. Then there is no steam and this wont influence my measurements. I made a reference measurement with an infrared thermometer and compared it to the measurements of the grid-eye sensor.

 

Here is a photo of the setup with the thermometer:

image

The Raspberry Pi with camera and grid-eye sensor took the following image (you can see my hand with the infrared thermometer in the screenshot; this did not influence the measurement negatively):

image

So the temperature in the pot was about 75 degrees celsius (according to the infrared thermometer, which always delivered reasonable values in the past). But the grid-eye sensor only measured 60 degrees celsius. So there is also a difference of about 15 degrees when heating oil.

 

Conclusion 1: the measurement is not influenced by the steam

Conclusion 2: I have to use some kind of calibration to calculate accurate temperature values.

  • Sign in to reply
Parents
  • aspork42
    aspork42 over 8 years ago

    Hello - I'm curious how much effect the neighboring pixels have. In other words; I wonder if the field of view for each "pixel" really overlaps. You've posted some amazing videos from the dual camera setup and they are kind of telling. In the previous video you posted, the temperature changes when you raise the pot up towards the camera. I think you may have success if you bring the camera closer to the cooktop so the pixels cover smaller areas.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • aspork42
    aspork42 over 8 years ago

    Hello - I'm curious how much effect the neighboring pixels have. In other words; I wonder if the field of view for each "pixel" really overlaps. You've posted some amazing videos from the dual camera setup and they are kind of telling. In the previous video you posted, the temperature changes when you raise the pot up towards the camera. I think you may have success if you bring the camera closer to the cooktop so the pixels cover smaller areas.