Pi Chef Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Pi Chef Design Challenge
  • More
  • Cancel
Pi Chef Design Challenge
Blog The Cooker Connector - Blog #2.5: A Slight Change of Plans (Pi Chef Challenge)
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
  • Author Author: jschools
  • Date Created: 30 Jan 2018 5:20 PM Date Created
  • Views 1568 views
  • Likes 9 likes
  • Comments 6 comments
  • pi chef
  • cooker connector
Related
Recommended

The Cooker Connector - Blog #2.5: A Slight Change of Plans (Pi Chef Challenge)

jschools
jschools
30 Jan 2018

Have you ever thought to yourself, “What a brilliant idea! I bet no one has ever thought of this before!”? That thought very rarely turns out to be true, and it just happened to me again. Oops.

 

Since writing my last post, I discovered that the company that makes my temperature probes released a new product that is basically a clone of what I'm building: https://www.thermoworks.com/Smoke-Gateway. I was shocked that I didn't find it when I was doing research before the contest, and I had been struggling with this dilemma for the past few days. I can't ethically reverse-engineer one of their products and then publish the steps to build a competing system. And, this clearly means that my contest entry is no longer a novel invention.

 

I emailed the Pi Chef Challenge organizers about this, and they were quick to respond. I proposed a modification to my design, and they said it was acceptable.

 

I am going to add a servo to open and close the air vents of my smoker. This will create a temperature feedback loop, enabling autonomous temperature control. This means that the smoker will be able to adjust its own temperature without the chef being involved! This is not a feature that the Smoke Gateway has, and I believe this will make my project more interesting and a novel concept again. (Fingers crossed!) It will still be connected to the cloud, the temperature graphs will still be displayed by the mobile app, and the vents will be controllable via the app as well. This obviously is an increase in scope, and in order to finish on time, I will be dropping the hands-free display portion of my original proposal as a trade-off.

 

Revised System Architecture:

image

 

Revised Project Plan:

The three components will need to be prototyped, designed and built in parallel. The first milestone is a Proof of Concept that demonstrates the end-to-end data path for real-time temperature information. Once I am confident that I can acquire temperatures and store them, I will build the servo system to control the air vents on the smoker. Once the prototype is functional, I will design and fabricate a PCB. Lastly, I will build the additional user features into the cloud back end and Mobile app. Below is a breakdown of the tasks for each component.

  • Monitor and Control Hub
    • Hardware component research
    • Hardware prototyping
    • Thermistor calibration
    • Software development to enable proof-of-concept
    • Servo system prototyping and building
    • PCB design and fabrication
    • NFC research and development
    • Enclosure prototyping and assembly
  • Cloud Back End
    • Database architecture development
    • Proof-of-concept development
    • Integration with Sensor Hub application
    • Integration with Android Client App
    • Cloud function and alerts development
  • Mobile App
    • Proof-of-concept development
    • Feature development

 

I’m actually pretty excited about adding this capability to my project, and I’m looking forward to this as a new challenge. I’m more of a software engineer than a mechanical engineer, so I’m definitely going to learn a lot from this modification. Look forward to some trial and error posts from me in the near future!

  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 8 years ago +5
    Interesting issue and ethics. Because someone else has a WiFi connected temperature sensor, it doesn't mean another company or individual can't do the same. If you were to use the same case and look, it…
  • genebren
    genebren over 8 years ago +4
    Jonathan, Interesting changes. There are quite a few PID controllers controllers out there that do something similar to what you are proposing. I did not do an exhaustive search, but what I saw were units…
  • e14phil
    e14phil over 8 years ago +4
    Great blog! I am glad you can adapt and move on, I find its the key to being most successful in life.
Parents
  • e14phil
    e14phil over 8 years ago

    Great blog!

     

    I am glad you can adapt and move on, I find its the key to being most successful in life.

     

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • e14phil
    e14phil over 8 years ago

    Great blog!

     

    I am glad you can adapt and move on, I find its the key to being most successful in life.

     

    image

    • Cancel
    • Vote Up +4 Vote Down