Experimenting with Polymer Capacitors
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Polymer Capacitors
  • More
  • Cancel
Experimenting with Polymer Capacitors
Blog Deep Dive into ESR, Testing
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: fmilburn
  • Date Created: 26 May 2019 12:26 AM Date Created
  • Views 7479 views
  • Likes 10 likes
  • Comments 14 comments
  • polymer capacitor
  • tenma 72-1020
  • capacitance measurement
  • esr measurement*
  • winners
  • esr
  • peak esr70
  • ad9850
  • capacitance
  • msp-exp430fr6989
Related
Recommended

Deep Dive into ESR, Testing

fmilburn
fmilburn
26 May 2019

The element14 Experimenting with Polymer Capacitors Challenge is an opportunity to “experiment, test, breadboard, or just play around with Polymer Capacitors” and then show what was learned.  In this second post the outcome of the experiments, results and findings for all of the Panasonic polymer capacitors in the element14 kit are presented.  Methods for improving the test procedure and potential further areas for study are discussed.

 

image

 

Background

 

While an ideal capacitor has no series resistance, Equivalent Series Resistance (ESR) exists in all real world capacitors, albeit with very small values in some of the polymer capacitors investigated here.  Two methods of measuring ESR will be used, the Peak ESR70 and an oscilloscope with square wave.  ESR is typically quoted at around 100 kHz which is where the Peak ESR70 operates.  In the 100 kHz range the capacitors being used in the this experiment begin to approximate a short circuit and inductance will be neglected.  With these assumptions, the voltage measured across the capacitor with an oscilloscope as shown in the following diagram is due to ESR.

image

In the introductory post the equation shown in the diagram was derived:

 

R = ESR = Vr (Rout) / (Vfg – Vr)     formula(1)

 

The updated experimental procedure is as follows:

 

Setup AD9850

  1. Set to 300 kHz
  2. Measure Rout using voltage divider equation with 100 ohm resistor replacing the capacitor
  3. Measure Vfg

Measure capacitance and ESR of each capacitor with the ESR70

  1. Measure and record ESR
  2. Measure and record capacitance

Measure capacitance of each capacitor with Tenma 72-1020 and Extech EX330

  1. Measure and record capacitance

Measure voltages of each capacitor with Siglent 1102 CML oscilloscope and 300 kHz square wave

  1. Measure and record open circuit voltage Vfg on oscilloscope
  2. Put the capacitor being tested in place as shown in the diagram
  3. Measure and record voltage across capacitor
  4. Look for exponential rise / fall due to RC charge / discharge and other anomalies

 

Calculate ESR with formula (1)

 

Measurement Notes

 

Measurement was done at approximately 22 degrees C and 60 % humidity. 

 

Peak ESR70

image

Measurement using the ESR70 is straightforward and easy.  The instrument is calibrated by holding the test button down until a prompt for probe compensation is received.  The clamps are shorted together and the measured resistance is then stored in the instrument and subtracted automatically from subsequent measurements.  In the photo above a 4.7 uF capacitor is being measured with the provided alligator clamps.  For the SMD parts it was found that the probe tips developed by jw0752 gave good contact and easily adapted to the ESR70 and can be used as shown below:

image

The ESR70 does not provide for Kelvin 4-wire measurement and the datasheet lists resolution as 0.01 to 0.02 ohms when ESR is below 2 ohms.  Readings varied from measurement to measurement during the experiment and a rough median is recorded in the raw data.

 

In the comments of the previous post there are a number of observations about the limitations of the ESR70 and suggestions for improving measurement of low ESR capacitors like those in this experiment.  These limitations will be apparent in the data presented.  Suggestions for improving measurement are presented at the end of this post.

 

Capacitance measurements from the ESR70 were reasonable but tended lower than the Tenma 72-1020 bench multimeter which has better specifications.  The other multimeter also gave somewhat higher readings than the ESR70 and was more in line with the Tenma.

 

Oscilloscope Method

 

A simple test fixture was developed for use with the oscilloscope method using 0.1 inch DuPont headers for the through hole capacitors and pads spaced from 0.1 to 0.3 inches at 0.1 inch intervals on protoboard for the SMD connectors.

image

A homebrew AD9850 Frequency Generator BoosterPack and a Texas Instruments MSP-EXPFR6989 LaunchPad were used to generate the square wave.

 

image

It was found that for some of the capacitors a frequency of 100 kHz resulted in excessive RC exponential behavior which improved when frequency was increased to 300 kHz.  Accordingly the readings with the oscilloscope method were taken with a 300 kHz square wave.  The output impedance of the AD9850 was measured to be 61 ohms.  In the photo below a 47 uF electrolytic capacitor is being tested.

 

image

 

In the photo below a 10 uF polymer capacitor is being tested.   For cans they were pressed against the pads.  Tantalum capacitors were also pressed against the pads although one smaller capacitor was soldered to see if it made much difference.  No error / difference between soldering and pressing in place was observed when care was taken to make good contact.

 

image

 

The oscilloscope test fixture suffers from resistance between the oscilloscope probe and the capacitor under test. The fixture had variable resistance depending on whether the Dupont header or pads were in use.  The additional resistance was estimated to be 0.008 ohms for the pads and this was backed out (similar to the way the ESR70 compensates for probe resistance).  Again, the measurement was not entirely repeatable. A rough median was recorded in the data table with high fliers excluded.

 

The oscilloscope screenshot below is from a 220 uF polymer aluminum electrolytic capacitor under test and indicative of very low ESR.  Because the voltage differential is so small this data point was not recorded in the table.

 

image

 

Inexpensive "MTester"

 

While performing the experiment I also received an inexpensive Chinese "MTester" based on the Atmel 328P that calculates among other things capacitance and ESR.  Here it is measuring a 33 uF polymer hybrid capacitor:

 

image

Note that it was incapable of measuring the ESR which was found to be around 0.04 ohms with the ESR70 and oscilloscope method.  The measured capacitance of 35.1 uF is close to what the other instruments reported.

 

Video Demonstration of Oscilloscope Method

 

The video below demonstrates how to use the oscilloscope method to measure ESR.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Raw Data

 

Data was recorded into the following spread sheet which automatically calculated ESR from the oscilloscope method as the data was entered.  All of the Panasonic polymer capacitors were examined and where available MLCC or electrolytic capacitors were available in the similar values they were also tested.  The resulting raw data is summarized in the table below.

image

Note that ESR was not recorded for those capacitors where ESR was at or below 0.03 ohms or so.  The ESR70 read 0.00 on these capacitors and the oscilloscope method was not considered reliable at such low levels as noted above.  Capacitance was measured with the ESR70 and the two digital multimeters.  The datasheet ESR is the maximum value.

 

Analysis of Capacitors Tested

 

image

All of the Panasonic polymer capacitors measured well within the specifications listed on the datasheet.  Measurement was at room temperature and the capacitors did not rise too much above room temperature.

 

Capacitance measurements between the ESR 70 and the Tenma 72-1020 bench multimeter were in good agreement although the ESR70 consistently measured lower than the Tenma 72-1020.

 

 

image

The measured ESR of the Panasonic polymer capacitors was at or below the maximum listed in the datasheet in all instances.  The maximum values listed in the table and plotted above for electrolytic capacitors are actually "typical" values from the ESR70 manual and in all cases the measured ESR was below these values.  However, due to inaccuracy in the testing methods at the very low ESR values the results should probably be looked at more as good or not-good for both the ESR70 and oscilloscope method.   The capacitors all appear to be good.

 

Some experimentation was done with frequency.  Increasing the frequency from 100 kHz to 300 kHz reduced the capacitive component.

 

Examination of the raw data table shows ESR of the electrolytic capacitors to be much higher than the polymer capacitors as expected.  A surprise was the relatively high ESR of the one SMD Multi Layer Ceramic Capacitor (MLCC) which is of unknown manufacture and came from a Chinese sample book.  This capacitor was also at the edge of its +/- 20 % capacitance specification.

 

Conclusion

 

The original objectives presented in the introduction were all met:

  • Describe ESR and how it can be measured
  • Obtain experimental ESR value for various capacitor types and values
  • Obtain experimental capacitance values for various capacitor types and values
  • Compare and summarize findings

 

The following conclusions were drawn from the experimentation:

  • The Panasonic polymer capacitors met the datasheet specifications for the conditions examined
  • Care must be taken in lead placement and contact when measuring ESR
  • The Peak ESR70 proved easy to use but does not have sufficient accuracy and precision for measuring ESR below about 0.04 ohms.
  • The oscilloscope method while more difficult to set up and slower to use produced results similar to the ESR70 when measuring ESR
  • An inexpensive "MTester" was unable to measure ESR for any of the polymer capacitors

 

There are several areas for improvement and further study:

  • Increasing the function generator voltage and thus current to the capacitor being tested would increase the voltage drop and thus improve ESR measurement with the oscilloscope method
  • A sine wave instead of a square wave (and some math) might allow investigation of the capacitive and inductive components
  • An improved oscilloscope test fixture with lower resistance and better contact for SMD components could be fabricated
  • Better measurement with an ESR meter would benefit from Kelvin 4-wire probes
  • Measurement of ESR at higher temperatures and over a range of frequencies would be interesting

 

Thanks for the interest - your comments, suggestions and corrections are always appreciated.

 

Corrections and Modifications

 

26 May 2019:  Corrected description of capacitor under test in low ESR oscilloscope screen shot - added the word polymer

6 June 2019:  Minor clarifying edits

 

Links

  • Deep Dive into ESR,  Introduction
  • Deep Dive into ESR,  Application
  • AD9850 Frequency Generator Booster Pack
  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 7 years ago +4
    Hi Frank, Thanks for the interesting report. I was fascinated by the different ways you approached the experiment. I have been using the M-Tester for rough measurements for some time and I have always…
  • fmilburn
    fmilburn over 7 years ago in reply to jw0752 +4
    Hi John, Thanks for the kind words. The tips worked great - they really grip and made good contact much easier on those SMD parts. I was thinking it would have been really neat if I could have affixed…
  • michaelkellett
    michaelkellett over 7 years ago +4
    Good stuff, Frank. I got my Taiwanese DE-5000 LCR meter via Ebay today. I paid £91.75 for it and then was stung for £24 by Royal Mail for £16 "tax" (VAT I suppose) and £8 "handling", I'll do a blog about…
  • fmilburn
    fmilburn over 7 years ago in reply to clem57

    Thanks Clem!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 7 years ago in reply to rscasny

    Hi Randall,

     

    Here are my thoughts:

    • There is educational value - the ESR70 is a box that gives a number.  Understanding the theory and applying it serves a useful pedagogical purpose.
    • By varying the frequency, or just observing the shape of the trace, it is possible to get further insight into other non-ideal behavior of the capacitor - e.g. inductance.
    • Using better equipment and applying some of the ideas listed in my conclusions would allow even more accuracy.

    Shabaz made a very interesting post on building a LCR meter here which I recommend that also has some very good comments below it.  Donald Lane posted a link to software that I was able to get working with the Keysight DSOX1102G oscilloscope I won in this contest (thank you very much image).   The software can generate a plot of ESR and Capacitance as a function of frequency and I posted an example in the comments.  Very enlightening and you can't get that kind of information from the ESR70.

     

    Frank

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • clem57
    clem57 over 7 years ago

    Nice report. I image the graphs. It takes time to collect all the points.

    Thumbs up.

    Clem

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rscasny
    rscasny over 7 years ago in reply to fmilburn

    Frank,

     

    I had someone contact me and asked about the oscilloscope method.

     

    Your wrote the o'scope method produced results similar to the ESR70. Would there be a situation where the o'scope method would be prefered even though it is slower to use and set up?

     

    Randall

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fmilburn
    fmilburn over 7 years ago in reply to phoenixcomm

    Hi Cristina,

     

    Great observation.  I would say knowing where to look for answers is 50% of being an engineer.  Realizing what the problem is that needs solving in the first place is what makes up the other 50%. image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
>