Experimenting with Polymer Capacitors
  • Challenges & Projects
  • Design Challenges
  • Experimenting with Polymer Capacitors
  • More
  • Cancel
Experimenting with Polymer Capacitors

Blog

  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New

Blog

  • Tags
  • Subscribe by email
  • More
  • Cancel
  • Capacitor Leakage Current over Temperature

    michaelkellett
    michaelkellett
    I was prompted to do this series of experiments by neuromodulator interesting blog posts. The puzzling thing abut his results is the apparent linking of rate of change of temperature with leakage current. I set up my own test arrangement using a...
    • 26 Jun 2019
  • Results and conclusion

    neuromodulator
    neuromodulator
    Results: Capacitance temperature dependence The first thing that I wanted to test was how the temperature affects the capacitance of the different capacitors. I performed a temperature sweep from ambient temperature to ~80 °C, and then back to a...
    • 19 Jun 2019
  • Introduction and methods

    neuromodulator
    neuromodulator
    Introduction Ideal capacitors can be defined with the following simple equation: In this design challenge I will explore parasitic elements of polymer capacitors that are not modeled by the previous equation, in particular I will explore ho...
    • 19 Jun 2019
  • more than you expect!

    COMPACT
    COMPACT
    Würth the effort!This challenge is an investigation about the viability of polymer capacitors and their use with vintage electronics.With the Panasonic SMT capacitor portion completed I was still looking for viable Polymer capacitors in through hole ...
    • 11 Jun 2019
  • Polymer Capacitors in Vintage Designs - Part #04

    COMPACT
    COMPACT
    LM3940-3.3 Linear Voltage Regulator With Polymer Capacitors The LM3940-3.3 is a linear voltage regulator that whittles down 5V to 3.3V.  This part was introduced for the proliferation of 3.3V parts and logic in the early 1990's.At first...
    • 9 Jun 2019
  • Polymer Capacitors in Vintage Designs - Part #03

    COMPACT
    COMPACT
    Further Improvements The photo shows the modifications I applied but this would not normally be done as a standard repair.It was purely an experiment applying first principles to improve system stability and reduce EMI. The modifications in...
    • 9 Jun 2019
  • Deep Dive into ESR, Application

    fmilburn
    fmilburn
    The element14 Experimenting with Polymer Capacitors Challenge is an opportunity to “experiment, test, breadboard, or just play around with Polymer Capacitors” and then show what was learned. In this 3rd and final post a Panasonic Polymer Capacitors f...
    • 6 Jun 2019
  • Using Polymer Capacitors for Supply De-coupling in the Current Amplifier - Test Results

    three-phase
    three-phase
    Introduction These are the test results from my experiments with changing out the electrolytic capacitors in the decoupling circuit of my current amplifier with alternative polymer capacitors. The test set up is described in the original bl...
    • 5 Jun 2019
  • Blog 2: As much as Polymer Capacitors can go in Instrumentation Amplifier.

    fyaocn
    fyaocn
    Contents Contents 01. Rating and Parameters of Polymer Capacitor in the Kits. 02. Simulation of AD8428 Instrumentation Amplifier by ADI 03. Schemtic Design and PCB Design 04. PCB making and Solding 05. Test with MKR1000 06. Conclusion &n...
    • 4 Jun 2019
  • Using Polymer Capacitors for Supply De-coupling in the Current Amplifier

    three-phase
    three-phase
    This is my unofficial entry into the Experimenting with Polymer Capacitors challenge - I never applied for the capacitor kit, as my little escapades into electronics are very ad hoc and I felt that a kit of capacitors would go to waste on me, and it ...
    • 30 May 2019
  • Polymer Capacitors in Vintage Designs - Part #02

    COMPACT
    COMPACT
    Can we remove this noise using polymer capacitors or by other means? As a random hack without applying any science I inserted some polymer capacitors at random into the PDN to observe any effects.I chose the capacitors with the most convenient p...
    • 27 May 2019
  • Evaluating Polymer Capacitors - Buck Converter Tests

    ralphjy
    ralphjy
    I've used a number of different buck converters to experiment with small solar panels.  Since this is a relatively short challenge I decided to modify an existing converter circuit rather than trying to design and build a new one.  Here...
    • 26 May 2019
  • Deep Dive into ESR, Testing

    fmilburn
    fmilburn
    The element14 Experimenting with Polymer Capacitors Challenge is an opportunity to “experiment, test, breadboard, or just play around with Polymer Capacitors” and then show what was learned.  In this second post the outcome of the ex...
    • 26 May 2019
  • Evaluating Polymer Capacitors - Pogo Pin Fixture

    ralphjy
    ralphjy
    The surface mount (SMD) capacitors used in this challenge are difficult to connect to instrumentation without soldering them into a test circuit.  To facilitate some of my scope and pulse generator measurements I made a simple test fixture that ...
    • 25 May 2019
  • Blog 1: Brief on Experimenting the performance of  Polymer Capacitors in Instrumentation Amplifier for Medical

    fyaocn
    fyaocn
    Experimenting the performance of  Polymer Capacitors in Instrumentation Amplifier for Medical 1. IntroducionMedical application like ECG use instrumentation amplifier to condition small signals in the presence of large common-mode voltages ...
    • 22 May 2019
  • Polymer Capacitors in Vintage Designs - Part #01

    COMPACT
    COMPACT
    I was most surprised to see my name in the Road Testers list.Totally unexpected!Many thanks to the sponsors and element14! I have encountered a lot of vintage electronic devices that make loud noises or produce smoke and glowing fireballs when p...
    • 20 May 2019
  • Evaluating Polymer Capacitors - Taking Some Data

    ralphjy
    ralphjy
    ESR70 measurementsThe first thing that I wanted to do was to use the ESR70 to measure the various capacitors in the kit.  This proved a bit challenging since these are all SMD parts.  The smaller flat capacitors were difficult even with the...
    • 20 May 2019
  • Experimenting with Polymer Capacitors - Basic Regulator Rewind

    rsc
    rsc
    I built a second set of circuits using MC78L05ACP regulators in a T092, and powered them up using a 9V battery.When I checked the outputs with no load (each powered separately), I found 1.9mv of noise on the non-poly cap circuit, and a 26mv 2.5khz os...
    • 15 May 2019
  • Experimenting with Polymer Capacitors - Basic Regulator

    rsc
    rsc
    I'm starting out with a simple regulator circuit as shown below:I built 2 circuits on prototyping pcb material, one with my regular caps, and one with the poly caps.When I checked the first circuit, the regulator was working fine with about +_2mv...
    • 14 May 2019
  • Evaluating Polymer Capacitors

    ralphjy
    ralphjy
    I was lucky to be selected as one of the sponsored challengers.  I received my kit last Tuesday but I was out of town, so I'm just getting started today. What's in the kitIncluded in the kit was a Peak atlas ESR+ model ESR70 meter a...
    • 13 May 2019
  • Experimenting with Polymer Capacitors - New Toys

    rsc
    rsc
    "Give a man a capacitor and he'll charge for a day, teach him to use an ESR meter and he'll spend all afternoon measuring stuff......" I compared the atlas ESR+ readings to my Fluke 87 DMM on a couple of my current hot film pow...
    • 13 May 2019
  • Polymer Cap Charge Pump

    dougw
    dougw
    IntroductionThis design challenge is about polymer capacitors - highlighting their features and applications. It is quite different to be focusing on a passive component in a design challenge, but it is a good exercise to become more familiar with po...
    • 12 May 2019
  • Deep Dive into ESR, Introduction

    fmilburn
    fmilburn
    The element14 Experimenting with Polymer Capacitors Challenge is an opportunity to “experiment, test, breadboard, or just play around with Polymer Capacitors” and then show what was learned.  I am grateful to be one of the competitors selected t...
    • 8 May 2019
  • Switched-Capacitor used in a Filter

    barsznica
    barsznica
    Hi all,My name is Pete and I have been a maker for many years. Well, I have been a "Breaker" for much longer!I though I could turn my passion into a job, so I completed a Degree in Electrical and Electronic Engineering. My experiment is to inves...
    • 16 Apr 2019