Products
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
Rocking Raspberry Pi
  • Challenges & Projects
  • Design Challenges
  • Rocking Raspberry Pi
  • More
  • Cancel
Rocking Raspberry Pi
Blog Issue and problem with the wolfson Audio
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: bharatrai888
  • Date Created: 5 Apr 2014 5:02 PM Date Created
  • Views 1825 views
  • Likes 0 likes
  • Comments 8 comments
  • rockingraspberrypi
  • raspberrypi
  • rocking_pi
Related
Recommended

Issue and problem with the wolfson Audio

bharatrai888
bharatrai888
5 Apr 2014

Hey Friend,


With excitement I want to thanks again to the element14 once again for the Wolfson Audio card. This week I got my Wolfson Audio Card delivered to my address. So thanks once again to element14 team and their staff for the support.


Now talking about the features of Wolfson Audio Card it was described earlier by me and also by other contestants.


It is unbelievably small in size and easy to attach with the Raspberry Pi. Unfortunately when it is interfaced we are unable to use Pi- Face control and display with the Raspberry Pi. Somehow this is the main disadvantage of the Wolfson Audio Card. Otherwise if talking about the audio usage of the raspberry pi as we have to design a karaoke machine, this one plays important role as we all are facing problems with the input audio problems as there has not any sound input capabilities. Other than that talking about the other disadvantages which might be I am facing is that for now the wolfson drivers are only available with pre-build image of the raspbian OS. So for now I changed my decision to use Raspbian OS.


So I’ve downloaded the build image of wolfson pi from Here.


Unluckily when writting the image file to memory card I got the error.


The image built has the larger size than that of the memory card. So I am unable to write the image to the memory card using win32diskimager.


The memory card we get has the storage capacity of 7.32 GB. But the built image has size approx 7.36 GB. So unluckily I am unable to write the image to the memory card. I am trying all sort of possible solution to write the data to it. Or otherwise I have to buy the memory card having capacity 16GB.


Do someone else facing the same issue?

  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 12 years ago +2
    Try this: Re: Wolfson modified Noobs raspbian zipped img Cannot unzip new download It's the standard Raspbian image with the Wolfson drivers patched in. The image is 2.8G, so should fit comfortably on…
Parents
  • AbhishekRao
    AbhishekRao over 12 years ago

    Hi Bharteindu,

     

    I have installed the build image of wolfson pi on a 16gb SD card and it works fine. Hence the best solution is to install the image in the 16GB Sd card. This will also give you a lot of space for recording audios and can get rid of compiling and installing the drivers and packages on the standard RASPBIAN. Kindly try this and it will definitely work as it has worked for me.


    Thanks,

    Abhishek

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • AbhishekRao
    AbhishekRao over 12 years ago

    Hi Bharteindu,

     

    I have installed the build image of wolfson pi on a 16gb SD card and it works fine. Hence the best solution is to install the image in the 16GB Sd card. This will also give you a lot of space for recording audios and can get rid of compiling and installing the drivers and packages on the standard RASPBIAN. Kindly try this and it will definitely work as it has worked for me.


    Thanks,

    Abhishek