Rocking Raspberry Pi
  • Challenges & Projects
  • Design Challenges
  • Rocking Raspberry Pi
  • More
  • Cancel
Rocking Raspberry Pi
Blog Issue and Problem with Wolfson Pi (Resolved)
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: bharatrai888
  • Date Created: 12 Apr 2014 6:01 PM Date Created
  • Views 1068 views
  • Likes 0 likes
  • Comments 2 comments
  • raspberry
  • rockingraspberrypi
  • rocking_pi
Related
Recommended

Issue and Problem with Wolfson Pi (Resolved)

bharatrai888
bharatrai888
12 Apr 2014

Hey Friend,



I was bit confused using the wolfson audio card. Somehow I am succeeded with the procedure described by Ragnar Jensen. A special thanks to him responding to every problem I’ve faced.


I tried every step described by him but still I failed. These steps involves all about replacing the kernel module with the kernel module built for the wolfson. But I am getting the error device or resource busy.

So I’ve decided to download the https://docs.google.com/file/d/0BzIaxMH3N5O1RUdSa19od1ltTjg/edit image build by Ragnar Jensen.



Hoping that might be this will fix the issue I am facing. Also praying that the wolfson I’ve got is not the faulty one. Also there is very less support for the wolfson from the developer team.



One is that the official built image is larger than the size of the memory card.



Other thing is that they are saying that they are working for the update so that one can update the kernel easily using the apt-get. But still it’s not working. This might be the great reason that most of us facing problem.



I am waiting that the team will soon announce something officially. So that installation of the wolfson audio card becomes easy for us and we have to not go through the steps which will lead to failure.

 

 

Edit: At last wolfson audio card worked as a charm. Heartily thanks to ragnar.jensen for providing the smaller size working Image for wolfson pi and going through my problem I've faced. Thanks again.

  • Sign in to reply
  • bharatrai888
    bharatrai888 over 12 years ago in reply to e14 Contributor

    Hi Rahul,

    You can download the image for wolfson pi from https://drive.google.com/file/d/0BzIaxMH3N5O1RUdSa19od1ltTjg/edit?usp=sharing .

    And the installation procedure is quite simple and is same like installing raspbian image.You can follow the steps from Raspberry Pi and Karaoke Machine (Wolfson Pi Installation) explained by babusingh9211. But instead of the official build image use the above image.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago

    Hi Bharteindu,

     

    Can you provide a link for the image for wolfson pi and installation procedure..