Products
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
Rocking Raspberry Pi
  • Challenges & Projects
  • Design Challenges
  • Rocking Raspberry Pi
  • More
  • Cancel
Rocking Raspberry Pi
Blog The Rocking Raspberry Pi Challenge - Part2- Karaoke Machine Overview
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: tech_kid
  • Date Created: 24 Feb 2014 2:35 PM Date Created
  • Views 707 views
  • Likes 2 likes
  • Comments 2 comments
  • sujith
  • sudhinalayam
  • rockingraspberrypi
  • raspberry-pi
  • raspberrypi-karaoke
  • rocking_pi
Related
Recommended

The Rocking Raspberry Pi Challenge - Part2- Karaoke Machine Overview

tech_kid
tech_kid
24 Feb 2014

Hello Friends,

     This is my second blog post on The Rocking Raspberry Pi Challenge about overview of the Karaoke Machine.

 

Introduction
     As part of the Rocking Raspberry Pi Challenge The Rocking Raspberry Pi Challenge (INDIA ONLY) I have to build a new type of Karaoke Machine which will test how well the Raspberry Pi Rocks using the video and sound capabilities of Raspberry Pi.


What is  Karaoke ?

     Karaoke is a form of interactive entertainment in which singers are sing along with the recorded music using a microphone and public address system. Lyrics are usually displayed on a video screen to guide the singer.

Source: Wikipedia

For more information please visit : Wikipedia.

 

Karaoke Machine using Raspberry Pi

     I have planned to build a Karaoke Machine as part of the challenge using Raspberry Pi and the following Hardwares which is provided by element14 for the Rocking Raspberry Pi Challenge.

  • Raspberry Pi Model B with 8Gb SD Card pre installed woth NOOBS
  • Pi-Face Control and Display
  • Wi-Pi

I will also use other hardwares  as follows which is need to build the Karaoke Machine.

  • USB Sound Card
  • Microphone

 

Software

     I have considered three Operating Systems such as – Raspbian, OpenELEC and RaspBMC to use in Raspberry Pi for my project and not yet finalized which one to use.

XBMC will be the main application/player will be used for Karaoke.


Karaoke Machine Features

   As of now I have planned to include the following features in my Karaoke machine project.

  • Playing Karaoke from music files in SD card or from any other media.
  • Playing Karaoke from Youtube
  • Playing Karaoke via streaming from Wifi or any other supported device.
  • Remote Control
  • Sign in to reply
  • tech_kid
    tech_kid over 12 years ago in reply to e14 Contributor

    Thanks, I am not fixed which OS to choose yet, as a newbee am trying these OS's as of now.

    Tried installing XBMC in Raspbian and it was a cumbersome task and didn't success.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago

    Nice post, but if you use raspbmc how will you use the piface ??