Rocking Raspberry Pi
  • Challenges & Projects
  • Design Challenges
  • Rocking Raspberry Pi
  • More
  • Cancel
Rocking Raspberry Pi
Forum Access to 5 GPIO pins with Wolfson Sound Card
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 4 subscribers
  • Views 2286 views
  • Users 0 members are here
  • wolfson
  • gpio
  • raspberry-pi
  • rocking_pi
Related

Access to 5 GPIO pins with Wolfson Sound Card

e14 Contributor
e14 Contributor over 12 years ago

Raspberry Pi provides GPIO on P1 and P5 connectors. Both these connectors are occupied by Wolfson Sound card.. Two on these GPIO are available on Wolfson card.  In our project we need 5 GPIO. Hence the two questions:

 

1. Of the GPIOs on P1 and P5 which ones are NOT used by the Wolfson sound card?

2. What is the best way to phyiscally accesses these GPIO.

 

We would not be able to use the Wolfson sound card if we do not get access to in total 5 GPIO pins. Please assist.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 12 years ago

    I am also interested in using some of the GPIO while using the Wolfson audio card. I have the card working, streaming audio from a server share over the network and it sounds very good. There is an "expansion header" shown on the photograph of the Wolfson audio card in the user documentation. However, there is no pin out for the "expansion header". There is, in the annexe, a table titled "e. Feature header signal assignment" that details the pin out for a 16 pin header. By a process of elimination (There is only one 16 pin header on the board!) I think the "Expansion header" and "Feature Header" are the same thing. If this is right, you have access to two GPIO connections and a range of audio connectors on this header. Just a shame the documentation is not more consistent.

     

    Anyone from Element 14 or Wolfson like to confirm that the Feature and expansion headers are the same thing and that he pin out is correct?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    Only two GPIO are available on header pins on the Wolfson card - UART0_TXD (GPIO14) and UART0_RXD (GPIO15).

     

    The Pi I2C does not route to the expansion header on the Wolfson card. If you want to connect a port expander I suggest soldering a 2 x 3 pin header to the top of the wolfson board at the Pin 1 end to make the I2C pins available to expansion boards and jumpers.

     

    I have soldered such a header and attached a RTC module to it. You could attach a gpio expander by jumper wires. Here is a photo showing the soldered header pins and RTC module. The flying leads from the RTC board connect to a GPIO expander.

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Marki555
    Marki555 over 12 years ago in reply to e14 Contributor

    Also GPIO3 on expansion header is available (connected to GPIO3 of WM5102 and to P1 pin 22 of RPi). I guess it can be used, else they wouldn't expose it on the expansion header.

    The P1 i2c is used to control the WM8804 SPDIF chip, but I see no issue in connecting another devices to the bus as suggested.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Marki555
    Marki555 over 12 years ago in reply to e14 Contributor

    Also GPIO3 on expansion header is available (connected to GPIO3 of WM5102 and to P1 pin 22 of RPi). I guess it can be used, else they wouldn't expose it on the expansion header.

    The P1 i2c is used to control the WM8804 SPDIF chip, but I see no issue in connecting another devices to the bus as suggested.