Rocking Raspberry Pi
  • Challenges & Projects
  • Design Challenges
  • Rocking Raspberry Pi
  • More
  • Cancel
Rocking Raspberry Pi
Forum All the Raspberry pi GPIO pins are occupied by Wolfson audio card... :( need access to GPIO :(
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 1 answer
  • Subscribers 5 subscribers
  • Views 2984 views
  • Users 0 members are here
  • wolfson_pi
  • rockingraspberrypi
  • raspberrypi
  • rocking_pi
  • wolfson_microelectronics
Related

All the Raspberry pi GPIO pins are occupied by Wolfson audio card... :( need access to GPIO :(

indiant3chi3
indiant3chi3 over 12 years ago

H3ll0  all !!

Is there any other way to access the Raspberry pi  GPIO pins ..?? Since all the pins are occupied by wolfson card need help image plzzz...

  • Sign in to reply
  • Cancel

Top Replies

  • rohitrangwani
    rohitrangwani over 12 years ago +1
    Check out these links rpi.gpio - Getting more than 26 GPIO pins - Raspberry Pi Stack Exchange Expand the Number of GPIO Pins on the Raspberry PI #piday #raspberrypi @Raspberry_Pi « adafruit industries…
  • e14 Contributor
    e14 Contributor over 12 years ago +1 suggested
    Two of the Raspberry's GPIO pins on the P1 header are made available on the Wolfson card. They are normally used as the UART serial console, but that function is easy to disable. http://www.hobbytronics…
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to indiant3chi3 +1
    Yes, most ultrasonic sensors I have seen use two GPIO pins. You can use the pins on the Wolfson card to connect it. -- Ragnar
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Two of the Raspberry's GPIO pins on the P1 header are made available on the Wolfson card.

    image

    They are normally used as the UART serial console, but that function is easy to disable.

    http://www.hobbytronics.co.uk/raspberry-pi-serial-port
    Raspberry Pi • View topic - Easily disable / enable serial console

    Then the two pins can be used as ordinary GPIO pins.

    --

    Ragnar

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Two of the Raspberry's GPIO pins on the P1 header are made available on the Wolfson card.

    image

    They are normally used as the UART serial console, but that function is easy to disable.

    http://www.hobbytronics.co.uk/raspberry-pi-serial-port
    Raspberry Pi • View topic - Easily disable / enable serial console

    Then the two pins can be used as ordinary GPIO pins.

    --

    Ragnar

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • indiant3chi3
    0 indiant3chi3 over 12 years ago in reply to e14 Contributor

    Hi Rangar!!!

    First of all thanks a ton for ur wolfson image contribution. And now thanks again for this GPIO clarification ... image . can i connect Ultrasonic sensor in this wolfson card  ? is that possible ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to indiant3chi3

    Yes, most ultrasonic sensors I have seen use two GPIO pins.

    You can use the pins on the Wolfson card to connect it.

    --

    Ragnar

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dimonic
    0 dimonic over 12 years ago in reply to e14 Contributor

    From the schematic, I take it that the audio card uses the i2c pins (1.3 and 1.5) on the header - can I still connect to these pins for another i2c device?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to dimonic

    Dominic Amann wrote:

     

    From the schematic, I take it that the audio card uses the i2c pins (1.3 and 1.5) on the header - can I still connect to these pins for another i2c device?

    Yes, you can. I2C bus is designed for multiple devices.