Save The Bees Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Save The Bees Design Challenge
  • More
  • Cancel
Save The Bees Design Challenge
Blog Bee Healthy - Blog 5: Edge Impulse Model
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Save The Bees Design Challenge to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ralphjy
  • Date Created: 19 Feb 2023 6:13 AM Date Created
  • Views 2493 views
  • Likes 18 likes
  • Comments 9 comments
  • save the bees
  • bee hive audio
  • savethebeesch
  • nicla vision
  • audio impulse design
  • edge impulse
  • buzz3 dataset
Related
Recommended

Bee Healthy - Blog 5: Edge Impulse Model

ralphjy
ralphjy
19 Feb 2023

I've selected the Buzz3 Audio Dataset to test model development and deployment to the Nicla Vision board using the Edge Impulse toolset.  I discussed this dataset in my previous post - Bee Healthy - Blog 4: Audio Dataset.

The Buzz3 dataset contains 11746 2sec samples split as follows:

train 
class hour min samples
bee 1 36 2880
cricket 2 0 3600
noise 1 24 2520
test
class min sec samples
bee 35 42 1071
cricket 19 14 577
noise 36 36 1098

I may end up rebalancing the training data, but I'll try it out first.  I already have an Edge Impulse account , so I just needed to create a new project that I named Bee_Present:

image

A great feature of the Edge Impulse Studio is the ability to upload existing data files provided they are in an accepted data format or file type.

Data Acquisition Formats:

  • CBOR
  • JSON
  • CSV

File Types:

  • WAV
  • JPG
  • PNG
  • AVI
  • MP4

The audio files in this dataset are all WAV files, so uploading the files with the appropriate labels was easy.

Data Acquisition

image

image

Impulse Design

For non-voice audio data it is generally recommended to use a Spectrogram Processing block - either linear or MFE (Mel-filterbank energy).  The MFE is designed to match human audio perception.  One might expect MFE to perform better because the data was labeled by human listeners.

image

I decided to try it both ways.

Audio (MFE) Impulse

image

Train the Neural Network:

image

The Quantized (int8) model accuracy is reasonable when validated against the training data:

image

But performs less well against the test data as would be expected:

image

Linear Spectrogram Impulse

image

Train the Neural Network:

image

Again, reasonable accuracy with the training data

image

But worse performance against the test data

image

Summary of Project versions:

image

The inference time of the Mel Spectrogram Impulse (35ms) is half of the Linear Spectrogram Impulse (71ms).  And it also has better memory efficiency and accuracy (with this dataset), so that's the model that I will use.

My first test when I get the Nicla Vision hardware will be to use the microphone to verify that I can do "Live classification" before I try to deploy the model.  

  • Sign in to reply
Parents
  • javagoza
    javagoza over 3 years ago

    When I have made live audio classifications I have had a problem with environmental noise and in the case of interiors with reverberation. It helps a lot to expand the samples with data augmentation and mixing samples with recordings of the ambient sound in which the system is going to be deployed.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ralphjy
    ralphjy over 3 years ago in reply to javagoza

    I agree with your comments and I may try to turn on data augmentation during training, but with this dataset I don't think that it will improve much.  It will be interesting to see how well live classification will work using audio data from this dataset captured by the Nicla Vision microphone.  There is a large problem with using out of context data (different hardware and setup), but it's not avoidable for this challenge.  And I don't think that I will have the opportunity to try this on an actual hive to get my own data.

    That being said, I'm amazed at how much effort is being made to capture beehive audio data.  It's just been hard to find usable data.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to ralphjy

    Do you think you would get any buzzing at the likes of a 'bee hotel' ? A bee hotel might be a bit more doable as an experiment at home than a hive.

    Spotted some on sale at the supermarket here yesterday but they were even more shallow than the ones already discussed here. Although to be fair they were being marketed as insect hotels rather than being solely for solitary bees. Might get a wider range of insect sounds however.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ralphjy
    ralphjy over 3 years ago in reply to beacon_dave

    I was actually discussing this project with a friend and discovered that his wife has started raising Mason bees.  In about a month she'll probably put out her cocoons saved from last year.

    I might try to get some audio recordings, but I think it will be difficult with an open structure with solitary bees (not sure where I would put the microphone).

    It would probably be easier to use image data with a "bee hotel".

    The other problem with audio data is the labeling.  I would probably need to do image capture correlated to the sound recording.  I'd need to do all of that using the Nicla Vision WiFi since LoRa does not have enough bandwidth.  I think that is out of scope for this challenge (at least for me).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to ralphjy

    I was thinking along the lines of a surface contact mic for a bee hotel scenario but there may not be much buzzing once the female bee lands and crawls into the opening, unless buzzing is used to drop off the pollen.

    Not sure what happens when the bees emerge from their cocoons. If you are the first egg to be laid at the far end of a long cavity, then there may be several bees ahead of you that need to leave before the exit is finally clear. Some buzzing might be going on there, perhaps for signalling or to test the wings readiness for exit flight.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ralphjy
    ralphjy over 3 years ago in reply to beacon_dave

    Not sure what happens in the wild, but people that raise mason bees "harvest" the cocoons in the late summer and store them in the frig until the next spring.  That's why the tubes are made to be replaceable. The cocoons are removed from the tubes which is a distructive process (to the tubes).  They put the cocoons out in the spring in the vicinity of the "bee hotel" (I've seen containers that are hung underneath).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • ralphjy
    ralphjy over 3 years ago in reply to beacon_dave

    Not sure what happens in the wild, but people that raise mason bees "harvest" the cocoons in the late summer and store them in the frig until the next spring.  That's why the tubes are made to be replaceable. The cocoons are removed from the tubes which is a distructive process (to the tubes).  They put the cocoons out in the spring in the vicinity of the "bee hotel" (I've seen containers that are hung underneath).