Save The Bees Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Save The Bees Design Challenge
  • More
  • Cancel
Save The Bees Design Challenge
Save the Bees DC Forum Have you used openmv and/or the Nicla Vision
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Save The Bees Design Challenge to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 78 subscribers
  • Views 6538 views
  • Users 0 members are here
Related

Have you used openmv and/or the Nicla Vision

scottiebabe
scottiebabe over 3 years ago

Openmv apparently adds a number of machine vision functions (like openCV) to micropython and includes a development IDE.

image

Source: https://docs.arduino.cc/tutorials/nicla-vision/blob-detection 

Recording a video clip is apparently as simple as:

import sensor, mjpeg, time

# Setup camera.
sensor.reset()
sensor.set_pixformat(sensor.RGB565)
sensor.set_framesize(sensor.QVGA)
sensor.skip_frames()
c = time.clock()

# Create the mjpeg object.
m = mjpeg.Mjpeg("example.mjpeg")

# Add frames.
for i in range(100):
    c.tick()
    m.add_frame(sensor.snapshot())

# Finalize.
m.close(c.fps())

Source: https://docs.openmv.io/library/omv.mjpeg.html 

You can also setup a rtsp server:

image

Any ideas for the save the bees design challenge... lol

  • Sign in to reply
  • Cancel

Top Replies

  • flyingbean
    flyingbean over 3 years ago +4
    One of biggest challenges is from the weather. It is winter at my city and there will have no bees until April/May next year. I can set up a camera outside of my house, burning a camera should be one less…
  • scottiebabe
    scottiebabe over 3 years ago in reply to flyingbean +3
    Yes, it is cold here too ! Even if the weather was warmer think I would still only demonstrate a proof of concept, but I have no ideas just yet. Excited to see what kind of solutions get proposed
  • javagoza
    javagoza over 3 years ago in reply to scottiebabe +3
    I don't know if I will be able to submit an application by the deadline. But if I present something, it will be with the idea of tackling a problem that affects bees, without the need to imply any contact…
Parents
  • javagoza
    javagoza over 3 years ago

    I have an OpenMV Cam H7 with which I was tinkering with OpenMV for a while in its early days.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago in reply to javagoza

    Very interesting! That board appears to have similar specifications to the nicla vision. Was using OpenMV similar to using openCV on a RPI?

    Did it work reliably or was it buggy and crash all the time?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • javagoza
    javagoza over 3 years ago in reply to scottiebabe

    When I was testing it, it was the beginning of that environment and I remember many crashes. But what made me most nervous was that the camera got very hot in a short time, so I stopped using it.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • javagoza
    javagoza over 3 years ago in reply to scottiebabe

    When I was testing it, it was the beginning of that environment and I remember many crashes. But what made me most nervous was that the camera got very hot in a short time, so I stopped using it.