Save The Bees Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Save The Bees Design Challenge
  • More
  • Cancel
Save The Bees Design Challenge
Save the Bees DC Forum Have you used openmv and/or the Nicla Vision
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Save The Bees Design Challenge to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 78 subscribers
  • Views 6538 views
  • Users 0 members are here
Related

Have you used openmv and/or the Nicla Vision

scottiebabe
scottiebabe over 3 years ago

Openmv apparently adds a number of machine vision functions (like openCV) to micropython and includes a development IDE.

image

Source: https://docs.arduino.cc/tutorials/nicla-vision/blob-detection 

Recording a video clip is apparently as simple as:

import sensor, mjpeg, time

# Setup camera.
sensor.reset()
sensor.set_pixformat(sensor.RGB565)
sensor.set_framesize(sensor.QVGA)
sensor.skip_frames()
c = time.clock()

# Create the mjpeg object.
m = mjpeg.Mjpeg("example.mjpeg")

# Add frames.
for i in range(100):
    c.tick()
    m.add_frame(sensor.snapshot())

# Finalize.
m.close(c.fps())

Source: https://docs.openmv.io/library/omv.mjpeg.html 

You can also setup a rtsp server:

image

Any ideas for the save the bees design challenge... lol

  • Sign in to reply
  • Cancel

Top Replies

  • flyingbean
    flyingbean over 3 years ago +4
    One of biggest challenges is from the weather. It is winter at my city and there will have no bees until April/May next year. I can set up a camera outside of my house, burning a camera should be one less…
  • scottiebabe
    scottiebabe over 3 years ago in reply to flyingbean +3
    Yes, it is cold here too ! Even if the weather was warmer think I would still only demonstrate a proof of concept, but I have no ideas just yet. Excited to see what kind of solutions get proposed
  • javagoza
    javagoza over 3 years ago in reply to scottiebabe +3
    I don't know if I will be able to submit an application by the deadline. But if I present something, it will be with the idea of tackling a problem that affects bees, without the need to imply any contact…
Parents
  • flyingbean
    flyingbean over 3 years ago

    One of biggest challenges is from the weather. It is winter at my city and there will have no bees until April/May next year. I can set up a camera outside of my house, burning a camera should be one less thing for my case, since cold weather can cool it down.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago in reply to flyingbean

    Yes, it is cold here too Snowman2! 

    Even if the weather was warmer think I would still only demonstrate a proof of concept, but I have no ideas just yet.

    Excited to see what kind of solutions get proposed Slight smile

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • rahulkhanna
    rahulkhanna over 3 years ago in reply to scottiebabe

    Perhaps it would be best to wait until April. However, it could be a fantastic idea to spend the next three months creating the prototypes and using them this summer.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago in reply to rahulkhanna

    It is a fair point. I am guessing the challenge won't actually start until mid-February or early March. I'm sure if you asked, the judging date could be postponed to date much closer to June/July to give challengers a chance to demonstrate their prototype with busy bees.

    Personally I don't intend to work with live bees Bee

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • javagoza
    javagoza over 3 years ago in reply to scottiebabe

    I don't know if I will be able to submit an application by the deadline. But if I present something, it will be with the idea of tackling a problem that affects bees, without the need to imply any contact with the bees during the project. It can be a project about any type of pollution, light, sound, electromagnetic, thermal... I don't know, I don't know very well the problems of bees and it would be a good opportunity to learn more about them.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago in reply to javagoza

    I am in a similar situation. I am unsure that I will know the problem and/or the solution to a bee problem in the next few days.

    My interest is really to experiment with the nicla vision and then in the final blog attempt to apply what I have learned to a bee problem.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • scottiebabe
    scottiebabe over 3 years ago in reply to javagoza

    I am in a similar situation. I am unsure that I will know the problem and/or the solution to a bee problem in the next few days.

    My interest is really to experiment with the nicla vision and then in the final blog attempt to apply what I have learned to a bee problem.

    • Cancel
    • Vote Up +3 Vote Down