Sci Fi Your Pi
  • Challenges & Projects
  • Design Challenges
  • Sci Fi Your Pi
  • More
  • Cancel
Sci Fi Your Pi
Blog Cybernetic Computer Interface - Almost done
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: sebathorus
  • Date Created: 28 Aug 2015 4:41 PM Date Created
  • Views 2072 views
  • Likes 4 likes
  • Comments 7 comments
  • cybernetic_interface
Related
Recommended

Cybernetic Computer Interface - Almost done

sebathorus
sebathorus
28 Aug 2015

Hello all

 

 

This is probably the last post I write before the end of "Sci Fi Your Pi" challenge and I want to take this occasion to thank Element14, sponsors and everyone involved in launching and managing this challenge and also for the opportunity to be part of it.

 

 

Although I did not manage to take this this project where I wanted, in this post I'll show you the current status of Cybernetic Computer Interface project.

For those of you not knowing what Cybernetic Computer Interface project is, please check the previous posts from here:

- Cybernetic Computer Interface

- Cybernetic Computer Interface - First step

- Cybernetic Computer Interface - Audio interface settings

- Cybernetic Computer Interface - Hardware description and functional demo

 

In the last post, you could see and hear Cybernetic Computer Interface in action operating inside a box. But Cybernetic Computer Interface is supposed to be a wearable device so let's make it so.

 

At this stage of construction, initial ideas about how mechanical structure should be made proved wrong and involved a lot of back and forth testing and redesign.

Because of the weight, in the end I had to add additional structural elements to make the device wearable.

One of the biggest problems was to put everything on the quite small frame.

 

The frame is built from aluminium strip, which is also light, flexible, strong and easy to work with. I need it to be flexible to allow the whole structure to

squeeze against the head and sit as tight as possible.

 

image

All boards are mounted on this frame with zip ties and wires in order to allow them to move without create mechanical tension in the boards, to avoid crack them.

 

The hardest point was to make the moving arm for Control and Display module. This should be mounted on the frame, must be extensible to allow an easy reading of display

and needs to be strong enough to not bend or break under the weight of CAD module (ask me how I know image ).

The actual version of the arm is made from a hacked selfie stick image

 

image

Also all power and control lines from RPi to CAD had to be long and flexible enough to allow mechanical parts to move. After trying MANY types of cables,

I end up using cables recovered from dead computer mice, which proved the best choice so far.

 

image

On the right side of CCI, I added two small voltage indicators, one for each LiPo cell. These have their own switch in order to be checked alone from the rest of the system.

 

Since the last post, the software was also improved with SDcard and USB drive support but voice recognition support is still not present.

 

Because of the large (and unforseen ) quantity of time involved in mechanical side development and building, I did not manage to build the outer shell and mount everything as I hoped for the final presentation, so this is the current state. Working but not finished.

I hope I will finish to build the outer shell in the next weeks and show you the completed device.

 

Here you can see different views of the device and a short demo movie.

image

 

imageimage

Aaaand my assistant beta testing the product image

imageimageimage

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

In the next weeks I'll build the outer shell and post here the final version with all planned features.

Thank you all for following Cybernetic Computer Interface building thread and I hope you found an interesting and informative journey.


All the best

-=Seba=-

  • Sign in to reply
Parents
  • DAB
    DAB over 11 years ago

    Looks good.

     

    You seem to have it balanced well and the display looks to be at a good height.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • sebathorus
    sebathorus over 11 years ago in reply to DAB

    Thank you

     

    The display arm and its positioning were one of the most difficult part of the mechanical side.

     

    -=Seba=-

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • sebathorus
    sebathorus over 11 years ago in reply to DAB

    Thank you

     

    The display arm and its positioning were one of the most difficult part of the mechanical side.

     

    -=Seba=-