Sci Fi Your Pi
  • Challenges & Projects
  • Design Challenges
  • Sci Fi Your Pi
  • More
  • Cancel
Sci Fi Your Pi
Blog Meditech: Battery test
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: balearicdynamics
  • Date Created: 18 May 2015 3:58 PM Date Created
  • Views 1434 views
  • Likes 1 like
  • Comments 13 comments
  • meditech_project
  • battery_test
  • pi_camera
  • scifi_your_pi
  • raspberry-pi
  • piface_dispaly2
  • battery_power
  • powering
Related
Recommended

Meditech: Battery test

balearicdynamics
balearicdynamics
18 May 2015

After a full-discharge the battery used for testing has been recharged with the simple circuit mentioned in the post Powering the camera probe for few hours to test if the charging circuit, experimental and very simple, may have problems .

 

Test conditionsimage

 

  • 7,5 Vcc / 1500 mA LiIon rechargeable battery
  • Full charge done (about 3 hours) with the LM350 based battery charger
  • Power regulator based on LM7805
  • Raspberry PI B+ with camera running continuously with the frame capture program.
  • Frames written on a NFS remote mount to have the WiFi connection always working
  • PiFace Display2 showing a continuously updated message (the system status test) and backlight enabled
  • The entire system has been packed with cardboard and exposed to almost hot sunlight

 

The duration time has been calculated from the power-on until one of the components has not presented problems due to the low power.

The entire system worked continuously for 63 minutes then camera continued to stream data but the LCD display backlight gone off and the Raspberry PI power led (the red one) disappeared.

The PI temperature shown on the display never raised more than 43 C

  • Sign in to reply

Top Comments

  • screamingtiger
    screamingtiger over 11 years ago +2
    I hereby propose we have an element14/sci fi your pi official get together at Enrico's house.
  • crimier
    crimier over 11 years ago +1
    Hi! It's nice to see your progress =) But I have to note that you shouldn't use a linear DC-DC (7805) for this purpose due to its inefficiency, as well as current limit. Use a switching regulator instead…
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to balearicdynamics +1
    Show off!! Who needs sunshine when you've got the glorious thunder and lightening like we've got here right now.. giving me goosebumps before I go on set
Parents
  • mcb1
    mcb1 over 11 years ago

    I just realised there was some electronics in the lower edge of the picture.

    Silly me ... I thought it was the view you were sharing .  image

     

    I wonder if you stopped the Backlight would your run time increase very much.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to mcb1

    Hello Mark,

     

    I see. I have used the backlight just to create a full consuming board image This should be avoided in most of the cases, sure.

     

    Anyway this battery charger / regulator should be totally revised for some implicit issues.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to mcb1

    Hello Mark,

     

    I see. I have used the backlight just to create a full consuming board image This should be avoided in most of the cases, sure.

     

    Anyway this battery charger / regulator should be totally revised for some implicit issues.