Sci Fi Your Pi
  • Challenges & Projects
  • Design Challenges
  • Sci Fi Your Pi
  • More
  • Cancel
Sci Fi Your Pi
Blog Meditech: Control panel PCB and circuit installation
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: balearicdynamics
  • Date Created: 9 Jun 2015 7:59 PM Date Created
  • Views 1283 views
  • Likes 2 likes
  • Comments 11 comments
  • meditech_project
  • alphanumeric_lcd
  • status_led
  • control_panel_assembly
  • pcb
  • calibration_potentiometer
Related
Recommended

Meditech: Control panel PCB and circuit installation

balearicdynamics
balearicdynamics
9 Jun 2015

PCB prototyping

After a final check the schematic is expected following the previous tests done with wires and breadboards so the final PCB prototype has been milled as shown in the images below.

imageimage

As shown in the final circuit assembled image, only the control components as soldered on the board (mainly the various pull-up resistors). As the board should be fit in the Meditech box and connected to the elements installed at different distances, all the other components are wires with connectors.

image

 

Installation

The following images shows how the board and the connections are set inside the box. The control components (LCD, LED status, IR Sensore and calibration potentiometer) are on the top side of the lid, accessible during the normal usage as it should remain closed (and possibly locked). The only two parts that remain inside of the box are the temperature sensor put in the RPImaster ares (the Raspberry-PI 2 main unit) and the can connection that is controled by the board. A couple of flat cables connect this control panel interface board to the ChipKit PI and another flat cable connects the board to the Raspberry PI GPIO for the IR sensor.

imageimage

 

Final view

The following images shows the final view of the control panel installed on the top side of the lid. The areas - actually empty - on both sides of the lid surface will include the plugs to connect the diagnostic probes, actually under construction.

imageimage

  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 11 years ago in reply to balearicdynamics +2
    Would that be like the axe my grandfather gave me .. I've replaced the handle a couple of times, and the head broke so thats been rerplaced as well... but its the same axe.
  • shabaz
    shabaz over 11 years ago in reply to mcb1 +2
    Hehe. We have a similar saying, called 'Trigger's Broom' : ) https://www.youtube.com/watch?v=BUl6PooveJE
  • fvan
    fvan over 11 years ago +1
    Excellent work as usual, Enrico!
  • fvan
    fvan over 11 years ago

    Excellent work as usual, Enrico!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<