Sci Fi Your Pi
  • Challenges & Projects
  • Design Challenges
  • Sci Fi Your Pi
  • More
  • Cancel
Sci Fi Your Pi
Blog Meditech phase 0 - Annex I: improving the eye probe camera
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: balearicdynamics
  • Date Created: 25 Aug 2015 11:05 PM Date Created
  • Views 1494 views
  • Likes 4 likes
  • Comments 6 comments
  • meditech_project
  • probe_improvement
  • raspberry-pi
  • evp
  • sci_fi_your_pi
  • image_patterns
  • camera_probe
Related
Recommended

Meditech phase 0 - Annex I: improving the eye probe camera

balearicdynamics
balearicdynamics
25 Aug 2015

Case design improvements

The Meditech eye probe camera is conceived to work nearby the main device component for easier usage. The camera position with the RGB light ring (see the image below) in the case prototype is fixed but need to be able to rotate and should be plied when the module is not in use to fit better in the component side of the case. This means to redesign this part of the case adding this two movements. As this part is the cover of the camera flat cable, it does not affect the circuitry and connections.

imageimage

Adding vision disease tests

Together to the active tests that can be done with the camera probe there is a series of test that can improve the vision potential diseases of the patient based on the use of the screen and special coloured patterns. The following images are two examples of the patterns used to generate VEP, Visually Evoked Patterns than can be used to record iris contraction and other secondary parameters, avoiding one of the associated analysis - The EEG - that need specialised personnel and can't be applied in the conditions usually expected for the Meditech device application.

imageimage

Another series of tests that should be implements with the esclusive use of the main color display are visual patterns to detect color blindness.

image

There is a consideration about this kind of tests. As apparently these can be useful only in certain kind of analysis and conditions, i.e. during a visit in an hospital, really the things are different. If we think the kind of environment the Meditech device is provided for, all the possible simple yet realiable diagnostic evaluations maybe useful at least for two reasons:

  1. Extend as much as possible the application possibilities offered by the device, increasing its versatility.
  2. Give the option to the medical operator to produce a patient investigation fast, simple and as much as complete possible.
  • Sign in to reply

Top Comments

  • amgalbu
    amgalbu over 11 years ago +1
    Hi Enrico The following images are two examples of the patterns used to generate VEP , Visually Evoked Patterns than can be used to record iris contraction and other secondary parameters, avoiding one…
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to amgalbu +1
    Hi Ambrogio, maybe I have explained not so well the concept. As a matter of fact, here I don't detect direct brain activity due the problem that and EEG is a complex analysis requiring well trained stuff…
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to screamingtiger +1
    Hi Joey, not these parts are faster and easier to make with the Mill machine. There are some parts instead like the temperature probe that are smoothed that will be done with 3D printer in the second testing…
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to screamingtiger

    Ha image

     

    Joey (or prefer Jack? John? Jim ? image image image), I am not rich nor unfortunately have so much toys. Simply on every paid client project I always keep apart something investing on my internal tools, components and evolution. Now a new project as started, that is related to the RoadTest I am publishing in these days, so say in touch. In the client budget I have planned a 500$-600$ for a 3D printer that is strategical for the project but is also strategical for Meditech and a lot of other cases to complete the option to ma a full working and well designed prototype.

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • screamingtiger
    screamingtiger over 11 years ago in reply to balearicdynamics

    You have too many nice toys image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to screamingtiger

    Hi Joey,

     

    not these parts are faster and easier to make with the Mill machine. There are some parts instead like the temperature probe that are smoothed that will be done with 3D printer in the second testing version of the Meditech.

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • screamingtiger
    screamingtiger over 11 years ago

    Did you 3D print those little parts?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to amgalbu

    Hi Ambrogio,

     

    maybe I have explained not so well the concept. As a matter of fact, here I don't detect direct brain activity due the problem that and EEG is a complex analysis requiring well trained stuff, usually a reasonable long time and a quite place to reduct almost all the external influences. But anyway there are secondary factors that interact in the body reactions in minor quantity. Some of these maybe useful to detect as least the suspect of some injuries that requires a more in-dept investigation. Then as Meditech can work in a cross referenced mode Some patterns also generate different answers in the ECG and heart beat. These are not definitive information but maybe useful. As I mentioned in the final phase zero post the fine tuning of this part of the VEP should be done with the support of a specialist I should meet probably next week.

     

    About the camera, for most of the physiological iris reaction time the camera frame rate maybe sufficient for a differential image check.

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
>