Sci Fi Your Pi
  • Challenges & Projects
  • Design Challenges
  • Sci Fi Your Pi
  • More
  • Cancel
Sci Fi Your Pi
Blog Meditech phase 0 - Annex III: The bluetooth printing protocol
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: balearicdynamics
  • Date Created: 27 Aug 2015 12:35 PM Date Created
  • Views 1592 views
  • Likes 2 likes
  • Comments 5 comments
  • meditech_project
  • graphic_printing
  • esc-pos_print_protocol
  • raspberry-pi
  • esc-pos
  • printing
  • bluetooth_printing
  • sci_fi_your_pi
  • thermal_printer
  • bluetooth_connection
Related
Recommended

Meditech phase 0 - Annex III: The bluetooth printing protocol

balearicdynamics
balearicdynamics
27 Aug 2015

This is a part that has not yet considered in the software development discussions.image

 

Introduction

As mentioned in a previous post, one of the Meditech peripherals is a small bluetooth 55mm thermal printer, covering a fundamental role, especially in cases of first aid and urgent interventions on-field.

The immediate following procedure expected after the very first aid operations with the help of the Meditech diagnostic probes is moving the patient in a organised structure for his hospitalisation or more adequate treatments.

 

As all the Meditech operated interventions are monitored and stored on a database, while every record is attached to the GPS absolute position and the precise synchronised date and time, it is possible to generate a short yet complete printout that will describe the patient health status, that will follow him during his transportation.

 

The first and most important use of these information is to give a summarised bunch of data in a human readable form (fast and reliable) to the doctors and specialised equipe that will support the patient.

The secondary but not less important reason is to keep a documented track on paper of the followed procedure by the first-aid personnel and the afforded strategy, if the patient has been moved, where he was recovered etc. In any case this track represent a testimonial document (that can be further integrated with the more complete diagnostic information stored on the Medited database) following the patient along his path.

 

There is also another important factor to consider: the availability of a printer can be extremely helpful to produce in any moment specific diagnostic data (e.g. the ECG track, the statistical results of a long period monitoring etc.). The availability of these information in a traditional paper support can be a key factor in certain conditions.

 

Printing more than text-only data

The Meditech Bluetooth printer works with the widely diffused ESC protocol, or Epson Escape, adopted by almost all the thermal roll printers (also named receipt-printers) by years. This protocol has been created by Epson around the en of 1980 and is actually one of the most reliable methods used by thermal printers. For more details on how the ESC protocol works see the following link on Wikipedia. The full (and few redundant) protocol specification from Epson is detailed in the attached document in pdf format.

While the protocol itself resulted a market winner adoption because of its simplicity its use is not so simple as it seems; as a matter of fact any control command should be sent to the printer in the form of and escape sequence resulting in a complex and difficult to debug code. Another issue approaching this printing protocol directly is its rigidity; every kind of different string should be managed properly taking in account that not all the printers - also supporting the same protocol - are the same and some control codes that works fine on a device can produce unattended effects on another.

 

Making a protocol parser

To solve the problem one for all it has been implemented a protocol parser, where every command has been converted in a simple function call accordingly with the following rules:

 

  1. Commands never generates printing mistakes or errors: if the required parameters are incomplete and it is not possible to apply a default value, the command should have no effect in the printout
  2. Commands should not send wrong data to the printer in any case
  3. Commands should be called in-line
  4. Commands should always return the expected value or an empty string (not NULL)
  5. Every command function should make a complete consistency check to avoid wrong escape sequences sent to the printer.

 

The resulting printing mechanism is dramatically simplified enabling the program to work with strings where the control code should simply be appended. So, for example to make a text in bold, there is the boolean call Bold( [ [true], false] ) returning the correct sequence to enable or disable the bold character: the string

 

"This is a BOLD test"

 

can be done as

 

"This is a " + protocolClassInstance.Bold(true) + "BOLD" + protocolClassInstance.Bold(false) +" test";

 

The same method will be applied to all. The following scriptlet shows the protocol class ESC_Protocol with all the available API; the full code will be posted in the GitHub repository.

 

class ESC_Protocol {

  public:
  int charSet;
  bool underline;
  bool bold;
  bool strong;
  bool reverse;
  bool bigFont;
  bool doublePrintHeight;
  bool doublePrintWidth;
  bool bitmapHighDensity;
  bool printHRI;
  int printHRIStyle;

  ESC_Protocol(void);
  ESC_Protocol(bool, bool, bool, bool);

  char* ResetPrinter();
  char* Bold(bool);
  char* CustomEsc(int[], int);
  char* Underline(bool);
  char* Underline(int);
  char* Reverse(bool);
  char* PrintAndFeedLines(int);
  char* EndParagraphLines(int);
  char* PrintAndFeedDots(int);
  char* CharTypeFace(int);
  char* HriTypeFace(int);
  char* CharBoundary(int, int);
  char* CharAttributes(int, bool, bool, bool, bool);
  char* AbsolutePosition(int);
  char* PrintingAreaWidth(int);
  char* CharacterScale(int, int);
  char* SelectPaperSensorStop(bool, bool);
  char* SetPanelButtons(bool);
  char* HorizontalTab();
  char* RelativePosition(int, bool);
  char* pagemodeAbsolutePrintPosition(int);
  char* pagemodeRelativePrintPosition(int, bool);
  char* DefaultLineSpacing();
  char* pagemodeFormFeed();
  char* pagemodePrintPage();
  char* NewLine();
  char* LineSpacing(int);
  char* RightCharSpacing(int);
  char* CharSpacing(int);
  char* HriPrintingPosition(int);
  char* BarcodeHeight(int);
  char* BarcodeWidth(int);
  char* Barcode(int, char*);
  void setDefaultSettings();
  void setBitmapDensity(int);
  void setCharAttributes(bool, bool, bool, bool, bool);
  void setCharTypeFace(int);
  void setCharBoundary(int, int);
  void setDotSpacing(int);
  void setLineSpacing(int);
  void setCharSpacing(int);
  char* getBoundary();
  char* getPrintableString(char*);
  char* getBitmapHeader(int, int, int);
  char* UserCharacterSet(bool);
  char* SetHorizontalTabs(int[]);
  char* DoubleStrike(bool[]);
  char* pagemodeSetPageMode();
  char* InternationalCharacterSet(int);
  char* pagemodeStandardMode();
  char* pagemodePrintDirection(int);
  char* pagemodePrintingArea(int, int, int, int);
  char* Rotate90(bool);
  char* SetMotionUnits(int, int);
  char* Justify(int);
  char* OpenCashDrawer(int);
  char* OpenCashDrawer(int, int, int);
  char* CharacterCode(int);
  char* CutPaper(int);
  char* UpsideDown(bool);
  char* LeftMargin(int);
  char* KanjiPrintMode(bool, bool, bool);
  char* SelectKanji();
  char* CancelKanji();
  char* KanjiUnderline(int);
  char* KanjiCharacterSpacing(int, int);
  char* KanjiQuadMode(bool);
  char* stringForPrinter(int[], int);
  char* pagemodeCancelPrintData();
  char* DoubleStrike(bool);
  char* Start();
  char* Max_Peak_Current_324(int);
  char* Max_Speed_324(int, int);
  char* Intensity_324(int);
  char* Status_324();
  char* Identity_324();
  char* Set_Serial_324(int);
  char* EOP_Opto_Type_324(int);
  char* EOP_Opto_Calib_324(int, int);
  char* EOP_Opto_Param_324();
  char* EOP_Opto_CurrLev_324();
  char* Save_User_Param_324();
  char* Factory_Default_324();
  char* Loading_Pause_324(int);
  char* Loading_Length_324(int, int);
  char* Loading_Speed_324(int, int);
  char* Historic_Heat_324(bool);
  char* Msk_App_324(int, int);
  char* Near_EOP_Presence_324();
  char* Near_EOP_Opto_Calib_324();
  char* Near_EOP_Status_324();
  char* Near_EOP_Opto_Curr_Lev_324();
  char* Internal_Font_324(int);
  char* Max_Columns_324(int);
  char* Text_Line_Rotate_324(bool);
  char* Paper_Forward_324(int);
  char* Paper_Backward_324(int);
  char* Graphic_Offset_324(int, int);
  char* Graphic_Print_324(int, int, int, char);
  char* Partial_Cut_324();
  char* Full_Cut_324();
  char* Barcode_Rotate_324(bool);
  char* Mark_Length_324(int);
  char* Tof_Position_324();
  char* Mark_To_Tof_Position_324(int, int);
  char* Opto_Head_Line_Len_324(int, int);
  char* Mark_To_Cut_Position_Len_324(int, int);
  char* Head_Dot_Line_ToCut_324(int, int);

};

Attachments:
imageescp2ref.pdf
  • Sign in to reply
Parents
  • shabaz
    shabaz over 11 years ago

    Hi Enrico,

     

    Thanks for this very useful information! Does the printer look like a serial interface/COM port over the bluetooth connection or something?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 11 years ago

    Hi Enrico,

     

    Thanks for this very useful information! Does the printer look like a serial interface/COM port over the bluetooth connection or something?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to shabaz

    Hi Shabaz,

     

    yes the hardware connection is serial. As a matter of fact there are several options for connecting this kind of printers: Bluetooth, USB, RS232 and LAN. Despite the LAN connection that is more complex in terms of cabling all the other alternatives will go to the internal serial connection approach. The use of Bluetooth is useful because gives mobility to the printer in a short range (between 5 and 10 m max and the printer can be locked to the belt.

     

    Enrico